RTCS detecting remote side close on a socket

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RTCS detecting remote side close on a socket

跳至解决方案
3,045 次查看
pmt
Contributor V

How do I detect if the remote endpoint is closed, or issued a shutdown request without actually reading or writing data to the socket (or using a KEEPALIVE which is only a polled test)?  I.E. how do I determine the socket state?

'RTCS_selectset(s, 1, -1) == s' tells me if "Data or shutdown request is initiated by remote endpoint or all sent data are acknowledged", but how do I determine which one (shutdown or data ack)?

Thanks,

PMT

标签 (1)
标记 (5)
0 项奖励
回复
1 解答
2,336 次查看
Martin_
NXP Employee
NXP Employee

RTCS_selectset() cannot return you this information, as it has just one return value, which is socket handle. Latest RTCS already has BSD-like select() function and it can distinguish between data requests/ close or reset requests/ acknowledge received for send data. It is part of the Freescale MQX for Kinetis SDK, and also will be in next MQX classic.

In "older MQX" you need to use other RTCS functions. recv()/send() functions give you an error when remote endpoint is reset/connection closed, example:

    retval = recv(sock,...);

    if(retval < 0)

    {

      uint32_t error_code = RTCS_geterror(sock);

      /* this might be for example RTCSERR_TCP_CONN_RLSD or RTCSERR_TCP_CONN_RESET */

      ....

      RTCS_shutdown(sock, 0); /* complete graceful connection close. destroy socket. */

      sock = RTCS_SOCKET_ERROR;

    }

Personally I would use RTCS_selectset() only on listening sockets to block wait for connection requests. If you like non-portable customization, you can just read the state from the TCB of a valid TCP socket:

  struct tcb_struct *tcb = ((struct socket_struct *)sock)->TCB_PTR;

  if(NULL == tcb)

  {

    /* connection is released -> reset, abort */

  }

  else

  {

     uint16_t tcp_state = tcb->state;

     /* it will be one of states defined in tcp_prv.h:

      * TCB states */

#define LISTEN         0

#define SYN_SENT       1

#define SYN_RECEIVED   2

#define ESTABLISHED    3

#define FINWAIT_1      4

#define FINWAIT_2      5

#define CLOSE_WAIT     6

#define CLOSING        7

#define LAST_ACK       8

#define TIME_WAIT      9

#define CLOSED        10

#define BOUND         11

*/

  }

Martin

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,337 次查看
Martin_
NXP Employee
NXP Employee

RTCS_selectset() cannot return you this information, as it has just one return value, which is socket handle. Latest RTCS already has BSD-like select() function and it can distinguish between data requests/ close or reset requests/ acknowledge received for send data. It is part of the Freescale MQX for Kinetis SDK, and also will be in next MQX classic.

In "older MQX" you need to use other RTCS functions. recv()/send() functions give you an error when remote endpoint is reset/connection closed, example:

    retval = recv(sock,...);

    if(retval < 0)

    {

      uint32_t error_code = RTCS_geterror(sock);

      /* this might be for example RTCSERR_TCP_CONN_RLSD or RTCSERR_TCP_CONN_RESET */

      ....

      RTCS_shutdown(sock, 0); /* complete graceful connection close. destroy socket. */

      sock = RTCS_SOCKET_ERROR;

    }

Personally I would use RTCS_selectset() only on listening sockets to block wait for connection requests. If you like non-portable customization, you can just read the state from the TCB of a valid TCP socket:

  struct tcb_struct *tcb = ((struct socket_struct *)sock)->TCB_PTR;

  if(NULL == tcb)

  {

    /* connection is released -> reset, abort */

  }

  else

  {

     uint16_t tcp_state = tcb->state;

     /* it will be one of states defined in tcp_prv.h:

      * TCB states */

#define LISTEN         0

#define SYN_SENT       1

#define SYN_RECEIVED   2

#define ESTABLISHED    3

#define FINWAIT_1      4

#define FINWAIT_2      5

#define CLOSE_WAIT     6

#define CLOSING        7

#define LAST_ACK       8

#define TIME_WAIT      9

#define CLOSED        10

#define BOUND         11

*/

  }

Martin

0 项奖励
回复
2,336 次查看
pmt
Contributor V

Martin,

Thanks!  I'm glad to see the full BSD select functionality coming in the next release.  For my reference, this is after MQX 4.1.1, correct?

0 项奖励
回复
2,336 次查看
Martin_
NXP Employee
NXP Employee

Correct, after MQX 4.1.1.

0 项奖励
回复