Protected Management Frames (PMF) 80211W support?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Protected Management Frames (PMF) 80211W support?

2,269 Views
hungjerry
Contributor II

Dear Sir,

  I wonder that if sabresd_6dq support 802.11w (pmf), I tried  modfied driver to add pmf feature and set right option in wpa_supplicant.conf while using the wpa_supplicant which complied with 11W function but no work,is there something i have to modify?

                              B.R jerry

0 Kudos
Reply
1 Reply

1,953 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hung

yes BCM4339 used in BSPs as stated in   Linux L4.14.98_2.0.0 Documentation

supports  IEEE 802.11w — Secure Management Frame according to its datasheet

http://www.mouser.com/ds/2/100/Radio%20with%20Integrated%20Bluetooth%204.1%20and%20FM%20Receive-9616... 

One can post question on murata support portal how to enable it

wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply