Problem using partition manager on eMMC device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem using partition manager on eMMC device

Jump to solution
3,587 Views
antonsvensson
Contributor I

Hi!

I'm trying to partition my eMMC memory using two partition managers.

I now have the problem that I'm only able to create the second partition on a specific place on the eMMC card. Otherwise it will timeout.

This is the relevant code snippet for partitioning.

        /* Open SD-CARD driver. */

        errorCode = fs_openComDrv(&pEmmcHandler,&pSdCardHandler, BSP_SDCARD_ESDHC_CHANNEL, sdCard, readOnly);

       

        /*Open Partitionmanager. */

        if(errorCode == MQX_OK)

        {

            errorCode = _io_part_mgr_install(pSdCardHandler,fs_PARTMAN_NAME1, 0);

            errorCode = _io_part_mgr_install(pSdCardHandler,fs_PARTMAN_NAME2, 0);

        }

       

        pPartManLog = fopen(fs_PARTMAN_NAME1, NULL);

        pPartManSecondary = fopen(fs_PARTMAN_NAME2, NULL);

       

        PMGR_PART_INFO_STRUCT part_info;

        uint32_t param;

       

        /* 42 Megabyte partition. */

        part_info.SLOT = 1;

        part_info.TYPE = PMGR_PARTITION_FAT32;

        part_info.START_SECTOR = 32;

        part_info.LENGTH = 8443000 - 64;

        param = 1;

        errorCode = ioctl(pPartManLog, IO_IOCTL_CLEAR_PARTITION,

                           (uint_32_ptr) &param);

        errorCode = ioctl(pPartManLog, IO_IOCTL_SET_PARTITION,

                           (uint_32_ptr) &part_info);

       

        /* 42 Megabyte partition. */

        part_info.SLOT = 2;

        part_info.TYPE = PMGR_PARTITION_FAT32;

        part_info.START_SECTOR = 8443000;

        part_info.LENGTH = 84430;

        param = 2;

        errorCode = ioctl(pPartManSecondary, IO_IOCTL_CLEAR_PARTITION,

                           (uint_32_ptr) &param);

        errorCode = ioctl(pPartManSecondary, IO_IOCTL_SET_PARTITION,

                           (uint_32_ptr) &part_info);

        param = 1;

        //errorCode = ioctl(pPartManLog, IO_IOCTL_VAL_PART, &param);

        errorCode = _io_mfs_install(pPartManLog, fs_FILE_SYSTEM_NAME, param);

        param = 2;

        //errorCode = ioctl(pPartManLog, IO_IOCTL_VAL_PART, &param);

        errorCode = _io_mfs_install(pPartManSecondary, fs_FILE_SYSTEM_SECONDARY, param);  

         pSdCardFsLogs = fopen(fs_FILE_SYSTEM_NAME, NULL);

        (void)ioctl(pSdCardFsLogs, IO_IOCTL_DEFAULT_FORMAT, NULL);  

         pSdCardFsSecondary = fopen(fs_FILE_SYSTEM_SECONDARY, NULL); <-- This will fail if I change the start_sector.

        (void)ioctl(pSdCardFsSecondary, IO_IOCTL_DEFAULT_FORMAT, NULL);

It will fail on the esdhc_read command.

        /* data is word aligned, maximize speed by copying directly from the register */     

        while (remains >= 4)

        {

            if (esdhc_ptr->IRQSTAT & (SDHC_IRQSTAT_DEBE_MASK | SDHC_IRQSTAT_DCE_MASK | SDHC_IRQSTAT_DTOE_MASK))

            {

                esdhc_ptr->IRQSTAT |= SDHC_IRQSTAT_DEBE_MASK | SDHC_IRQSTAT_DCE_MASK | SDHC_IRQSTAT_DTOE_MASK | SDHC_IRQSTAT_BRR_MASK; <--- Fails here, the DTOE flag is set after the first byte is read.

                return IO_ERROR;

            }

Anyone else that have had problems using eMMC and partitioning?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,740 Views
antonsvensson
Contributor I

The problem did not lie in the way I opened the device.

The problem was that I had initialized the device with byte addressing but it should have been addressed with block addressing method.

The SDHC driver in MQX  is not returning a fault if you try to access outside the boundaries of the device, that gave me some problems when debugging, it will just stay silent and hang on that line.

Best regards

Anton Svensson

View solution in original post

0 Kudos
Reply
3 Replies
2,740 Views
RadekS
NXP Employee
NXP Employee

I see that you tried install partition manager twice.

I suppose that this could cause this issue.

You should install partition manager over SD card and subsequently open selected partitions. For example:

// Install partition manager over SD card driver

errorCode= _io_part_mgr_install (pSdCardHandler, "pm:", 0 );

pPartManLog = fopen ( "pm:1", NULL );

pPartManSecondary = fopen ( "pm:2", NULL );

//pm:0 is whole device; pm:1, pm:2, pm:3, pm:4 are partitions

Optionally you can use IOCTL command for selecting right partition:

// Install partition manager over SD card driver

errorCode = _io_part_mgr_install (pSdCardHandler, "pm:", 0 );

pPartManLog = fopen ( "pm:", NULL );

partition_number = 1;

error_code = ioctl(pPartManLog, IO_IOCTL_SEL_PART, &partition_number);

pPartManSecondary = fopen ( "pm:", NULL );

partition_number = 2;

error_code = ioctl(pPartManSecondary, IO_IOCTL_SEL_PART, &partition_number);

// partition_number=0 is whole device, 1, 2, 3, 4 are partitions


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,741 Views
antonsvensson
Contributor I

The problem did not lie in the way I opened the device.

The problem was that I had initialized the device with byte addressing but it should have been addressed with block addressing method.

The SDHC driver in MQX  is not returning a fault if you try to access outside the boundaries of the device, that gave me some problems when debugging, it will just stay silent and hang on that line.

Best regards

Anton Svensson

0 Kudos
Reply
2,740 Views
RadekS
NXP Employee
NXP Employee

Thank you for your notification about root cause.

0 Kudos
Reply