PHY KSZ8051MLL Integration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PHY KSZ8051MLL Integration

1,617件の閲覧回数
payyans4u
Contributor I

Hi,

 

I am currently working on MCF52259 with CW 7.2 ...i am using a PHY KSZ8051MLL...The demo kit that i have has  a Micrel 8041 NL PHY.....Do anyone here have a working knowledge of KSZ8051 MLL...or atleast if sumbody could tell me the difference between the two would be of great help....Thanks in advance

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,264件の閲覧回数
Weining
Contributor III

I am using the same things. the driver for the demo board (for 8041) works well for KSZ8051 on my board. I had talked to the Micrel applcation engineer, he mentioned that Micrel does not change any register addresses from 8041 to 8051.

 

the main difference between 8041 and 8051 might be the hardware,  you could check Micrel application note AN-143.