Hi,
I'm designing hardware that interfaces a K60P100M100 MCU with an Ethernet physical interface. I am looking for a reference design that includes the connection details of the PHY chip (such as a KSZ8041NL) to the K60, including the optimal configuration for clocks etc.... Probably an RMII rather than MII interface.
The TWR-SER board has lots of superfluous links and configuration options which I'm finding confusing as a reference design. For example I don't believe I would need the NB2304 clock distribution chip if both the MCU and PHY are running from a single 50MHz clock.
Some references have also indicated that the RMII mode is preferred as there is overlap on some devices with the JTAG interface.
Can anyone point me to a schematic for this already done on the same PCB? Help appreciated.
David
David,
There is only one pin multiplexed between JTAG and RMII_RXER. Pin 39 JTAG_TRST , RMII_RXER. RMII_RXER is optional pin for RMII interface and JTAG_TRST is optional for JTAG. I think you can use whatever funtion you like. There is an errata for some slicon version for RXER too.
I suggest you to check TWR-K60N512 kit reference. I have started a new design similar to one you have. I use K60N512.
Mehmet
Do check that if you are going to use USB, you will need the K60 to be running at 96MHz as the USB requires a clock of 48 MHz.
In the above setup the MII interface would require a separate clock. Not sure about RMII clock requirement, so do check on this.
Mohsin