Hi all,
My problem seems to be like this How to set up BSP for PEx in KDS
I'm using KDS2.0.0 and MQX_4_1.
I would like to build the pe_demo exemple to run on a twrk60f120m board.
The problem is that it requires a PEx based BSP and I'm not able to find it.
Where am I false ?
Thank you for the answers
PS: it seems OK when using CodeWarrior 10.6
Hello Philippe,
Please check the below thread and let me know if this helps !!!
https://community.freescale.com/docs/DOC-103429
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Sol,
Thank you.
As I wrote , I'm using TWRK60fK20m board.
The solution you proposed is based on SDK, and there is no SDK available for this board.
I saw that it is recommended to use a superset of the processor and to "adapt" the SDK.
But for this family, there are only two SDKs with a K64F and with a K60D, and none of them is a superset of K60F.
As I don't know how difficult it is ,I'm afraid not have enough time to create this new SDK.
What do you think about that ?
Best regards
Philippe