MQX4.2 GPRS connect error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MQX4.2 GPRS connect error

1,429 次查看
errsionjack
Contributor I

Hi everybody.

     I was suing the MQX4.2 to test the GPRS(C:\Freescale\Freescale_MQX_4_2\rtcs\examples\gprs).The printf information told me that the PPP is ok, but

resolve hostname was error. When I used the fix IP, the ping was error too.The GPRS module is ok, the model is M26(Quectel).My Paltform is K60D100M.Anybody can give me some suggestions?

 

DNS server added successfuly.

Connection established

Local address:  96.136.107.33

Remote address: 0.0.189.50

 

PPP connection ok

GPRS modem connected successfuly

Trying to resolve hostname

Hostname resolution successful

Pinging on address:123.125.114.144

PING_ERROR: error = 0x1510

PING_ERROR: error = 0x1510

PING_ERROR: error = 0x1510

PING_ERROR: error = 0x1510

 

Trying to sync Time:

SNTP_ERROR: error = 0x1510

 

PPP connection closed

Original Attachment has been moved to: GPRS_TEST.zip

0 项奖励
回复
1 回复

1,122 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Jack,

I have not run tests with GPRS, but I made tests with a Win 7 PC creating a PPP connection and everything worked fine. You can find the instructions here:

How to Create a PPP Connection with MQX4.2 and Win 7

My advice is to test with the PC first, verify it works and then debug the application to follow the steps required for PPP configuration. After this you may reproduce the same in your application for GPRS.

Best regards,

Carlos

0 项奖励
回复