MQX10.3, where is the wizard to make a project?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX10.3, where is the wizard to make a project?

799 Views
CarlFST60L
Senior Contributor II

MQX10.3, where is the wizard to make a standard MQX3.8 project????

Mine only has MQX Lite included and all the bare board stuff, and linux...

I'm not using any of these project types, I just want standard MQX3.8 on a 52259evb... hard much?

0 Kudos
Reply
1 Reply

609 Views
Martin_
NXP Employee
NXP Employee

New project wizard for a Freescale MQX 3.8 project can be installed via CW 10.3 update site.

In CW 10.3, go to Help->Install New Software... and select the FSL MCU Eclipse Update Site as shown on the image below:

2012-10-05-CW_10_3_Install_New_Software.gif

Select MCU v10.3 Updates for MQX and Next > until installation starts. After it is finished, restart the CW 10.3. File->New menu now has the option to create MQX 3.8 Project.

0 Kudos
Reply