MQX v4.2 with VLE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX v4.2 with VLE

1,719件の閲覧回数
janos_murai
Contributor III

Hi,
I work with an MPC5644A MCU, which has an e200z4 dual issue core.
Can I compile the MQX v4.2 to VLE instructions? According to the linked doc (http://www.nxp.com/assets/documents/data/en/supporting-information/FSL_MQX_4_0_2_RN.pdf ), MQX is ported to e200 VLE, so I think it should work, but it doesn't. When the execution reaches the _mqx() function, it jumps to the Interrupt section and stucks. The first intruction in the _mqx() function is se_stb r2,4(rsp).
Although I'm not sure, that the problem is about the VLE instructions...

Any help in this topic is appreciated!

Thank you!
János Murai

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,551件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Unfortunately MQX 4.2 does not support PowerPC devices.
You need to use MQX4.0.2. this is the lastest version that supports PowerPC devices.

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,551件の閲覧回数
burakduzgun
Contributor I

Hi soledad, did you use mqx4.0.2 for PowerPC?

0 件の賞賛
返信