MQX missing BWT in MCF5225.h

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MQX missing BWT in MCF5225.h

940 次查看
carlnormansuret
Contributor V

When the next release happens can someone please update the mcf5225.h file to include the BWT (location Freescale_MQX_4_2\mqx\source\psp\coldfire)

Like this:

typedef struct mcf5225_struct

{

...

// unsigned char                     filler10[0x10000];

   MCF5225_WATCHDOG_STRUCT BWT; //ADD THIS PLEASE

...  

} MCF5225_STRUCT, * MCF5225_STRUCT_PTR;

typedef volatile struct mcf5225_struct * VMCF5225_STRUCT_PTR;

Would also be nice if you could change fatal errors etc to call a reboot like this

#define REBOOT_ON_FATAL_ERROR

and have

void _mqx_fatal_error

(

    _mqx_uint error

)

{ /* Body */

#ifdef REBOOT_ON_FATAL_ERROR

  VMCF5225_STRUCT_PTR reg_ptr = (VMCF5225_STRUCT_PTR)(0x40000000); //Multicom

  reg_ptr->CCM.RCR |= (1 << 7); //Multicom

#else

...

Same thing in

_int_unexpected_isr

1 回复

849 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Norman:

Thank you for your feedback. I will submit a feature improve request to the developer team.

Regards

Daniel