MQX RTCS Initialization procedure, difference between APIs starting with RTCS_ and ipcfg_

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX RTCS Initialization procedure, difference between APIs starting with RTCS_ and ipcfg_

1,121件の閲覧回数
sooraj
Contributor I

I am using 'twrk70f120m' and Freescale MQX RTOS with CodeWarrior IDE. Please help me to find answer for my doubts regarding MQX RTCS.

In MQX RTCS User Guide I could find APIs starting with RTCS_ and ipcfg_ what are the differences between these two.

As mentioned in the same document we can initialize Ethernet with APIs RTCS_create, ENET_initialize, RTCS_if_add and RTCS_if_bind, can I create a socket and communicate after initializing this way or is it required to do any thing else.

Is it possible to change MAC ID without restarting the device.

タグ(4)
0 件の賞賛
返信
0 返答(返信)