MQX_CORRUPT_STORAGE_POOL received for default "Timer Task"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX_CORRUPT_STORAGE_POOL received for default "Timer Task"

1,794件の閲覧回数
buddingspacer
Contributor I

For the default "Timer task", we recieve the POOL_BLOCK_IN_ERROR,

 and the MQX_CORRUPT_STORAGE_POOL  in get_mem_error(), this happens when the taks are heavily loaded and the used memory reaches about 92 %

 

MQX_CORRUPT_STORAGE_POOL , on what instances this can happen for a timer task,?

 

Usage Details

Timer component is created with its default priority & size.

_timer_create_component(TIMER_DEFAULT_TASK_PRIORITY,TIMER_DEFAULT_STACK_SIZE)

 

 

0 件の賞賛
返信
2 返答(返信)

1,583件の閲覧回数
c0170
Senior Contributor III

Hi buggingspacer,

 

can you please provide more details? Which MQX version, what board are u using? Perhaps some code snapshots. Things which could greatly help us to reproduce the error you received.

 

Regards,

MartinK

0 件の賞賛
返信

1,583件の閲覧回数
buddingspacer
Contributor I

MQX version is 2.407, and RTCS we use is 2.94. We are using a 68K processor -  MC68EN302

 

 

For Timer task callbacks we use system message pool of this size,

_msgpool_create_system(sizeof(SYSTEM_MSG), 100, 50, 250))

 

What more specific detail is required? Any suggestions on which area/part could be the root cause, so we can probe on that direction?

0 件の賞賛
返信