MQX 4 Release date?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,931件の閲覧回数
naftalir
Contributor III

Hi all,

is there anybody who knows when the MQX 4 will be released? "Early December 2012..." ? :/

Best Regards

1 解決策
3,499件の閲覧回数
BryGuyH
Contributor IV

Oh wow. I've just been checking Freescale MQX™ Software Solutions - Releases and Patches</title><meta name="... which still shows 3.8.1 as the latest and awaiting an email from my FAE. I didn't think to drill into the download pages to see if it was there. I'll try and see what I get.

Edit: You're right it is there on the downloads page. Currently downloading FSLMQXOS_4_0_0.exe 36.2/170MB, 4 mins left...

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
3,499件の閲覧回数
dspNeil
Contributor III

It's showing as available since 12/14 on the MQX page. I've been trying to grab it all day though, and the downloads just won't start.

3,500件の閲覧回数
BryGuyH
Contributor IV

Oh wow. I've just been checking Freescale MQX™ Software Solutions - Releases and Patches</title><meta name="... which still shows 3.8.1 as the latest and awaiting an email from my FAE. I didn't think to drill into the download pages to see if it was there. I'll try and see what I get.

Edit: You're right it is there on the downloads page. Currently downloading FSLMQXOS_4_0_0.exe 36.2/170MB, 4 mins left...

0 件の賞賛
返信
3,499件の閲覧回数
naftalir
Contributor III

It is realy exists in the Download Page :smileyhappy:

Thanks!!

0 件の賞賛
返信
3,499件の閲覧回数
Teckna
Contributor V

Hi,

I can see MQX 4.0 in the download page. But why MQX 3.8.1 was 490 MB and MQX 4.0 is 173 MB?

Many thanks

Teckna

0 件の賞賛
返信
3,499件の閲覧回数
Martin_
NXP Employee
NXP Employee

Hi Teckna,

MQX 3.8.1 installation contains pre-built MQX libraries (in the lib folder).

MQX 4.0 lib folder is almost empty after installation, users are required to compile MQX 4.0 libraries with their build tools. Also some BSPs have been completely removed from MQX 4.0, check release notes.

0 件の賞賛
返信
3,499件の閲覧回数
Teckna
Contributor V

Thanks for the answer, Martin

Teckna

0 件の賞賛
返信
3,499件の閲覧回数
BryGuyH
Contributor IV

That's code for January.

For example:

Re: IPv6 and SCTP

0 件の賞賛
返信