MQX 4.2 Missing CodeWarriorNPW folder

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX 4.2 Missing CodeWarriorNPW folder

1,451件の閲覧回数
danir_
Contributor I

Hi,

MQX 4.2 clones correctly with the BSPCloningWizard. But this update losts the reg32 & 64 files & xmls.

It is a bug ?

0 件の賞賛
返信
2 返答(返信)

1,291件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Dani,

Thank you for your bug report.

You are right, this feature missing in current version of BSP Cloning Wizard tool.

We changed type of generators (now it is ruby) and we miss this point.

I will report it into our internal bug database.

Note: *.xml and *.reg files are in readable format therefore you can edit them by any text editor.

I generated MY_BOARD411 BSP from frdmk64f BSP. You could take xml file, modify "MY_BOARD411" BSP name into your name and modify MCU type. In reg file you should replace "MY_BOARD411" by your BSP name and edit path to MQX4.2 with MQX version. After that, it should work even with MQX4.2

I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,291件の閲覧回数
danir_
Contributor I

Thanks, I used 4.1.1 files and I updated for 4.2.

0 件の賞賛
返信