MQX 4.2 Kinetis Serial DMA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MQX 4.2 Kinetis Serial DMA

2,853 次查看
kfranz
Contributor III

In MQX 4.2 there is a file named serl_dma_kuart.c

Freescale_MQX_4_2\mqx\source\io\serial\dma\serl_dma_kuart.c

Are there any examples that use DMA for the UART? I would like to change from the interrupt driven driver to one that uses DMA so that I can run at a higher baud rate.

Will using DMA reduce or eliminate serial port interrupts?

0 项奖励
回复
3 回复数

2,839 次查看
kfranz
Contributor III

No, UART DMA is not working.

Does anyone have any suggestions?

0 项奖励
回复

2,842 次查看
kfranz
Contributor III

I am using the K65. In:

C:\Freescale\Freescale_MQX_4_2\mqx\source\bsp\twrk65f180m\initbsp.c for ittya, I made the changes below:

#if BSPCFG_ENABLE_ITTYA
//_kuart_int_install("ittya:", &_bsp_sci0_init, _bsp_sci0_init.QUEUE_SIZE);
_kuart_dma_install("ittya:", &_bsp_sci0_init, _bsp_sci0_init.QUEUE_SIZE);
#endif

It seems to be working okay. I assume I am now using DMA?

0 项奖励
回复

2,822 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi kfranz:

The checked this, and the UART DMA is not documented.  It looks like the files were added for future release. But now MQX 4.x is replaced by MQX v5.  Please refer to below link for more details.

https://www.nxp.com/design/software/embedded-software/mqx-software-solutions/mqx-v5-software-solutio...

I would suggest you do more test on your side.

 

Regards

Daniel

 

0 项奖励
回复