MQX 4.2 K24 clock settings

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX 4.2 K24 clock settings

ソリューションへジャンプ
3,900件の閲覧回数
ryanlush
Contributor IV

I've noticed my clock is running slower than it should be. Inside of bsp_cm.c you have the following defines

/* Clock configuration 0 */
#define CPU_MCG_MODE_CONFIG_0                              (CPU_MCG_MODE_PEE | CPU_CLOCK_EXTERNAL_CRYSTAL_MASK | CPU_CLOCK_FAST_MASK) /* Clock generator mode */
#define CPU_CLOCK_VLP_CONFIG_0                             0U /* RUN power mode */

#define CPU_MCG_C1_CONFIG_0                                0x20U /* MCG_C1 */
#define CPU_MCG_C2_CONFIG_0                                0x25U /* MCG_C2 */
#define CPU_MCG_C4_CONFIG_0                                0x00U /* MCG_C4 */
#define CPU_MCG_C5_CONFIG_0                                0x03U /* MCG_C5 */
#define CPU_MCG_C6_CONFIG_0                                0x40U /* MCG_C6 */
#define CPU_MCG_SC_CONFIG_0                                0x02U /* MCG_SC */
#define CPU_OSC_CR_CONFIG_0                                0x80U /* OSC_CR */
#define CPU_SIM_SOPT1_CONFIG_0                             0x00080000UL /* SIM_SOPT1 */
#define CPU_SIM_SOPT2_CONFIG_0                             0x00010000UL /* SIM_SOPT2 */
#define CPU_SIM_CLKDIV1_CONFIG_0                           0x01130000UL /* SIM_CLKDIV1 */
/* Clock configuration 1 */
#define CPU_MCG_MODE_CONFIG_1                              (CPU_MCG_MODE_PEE | CPU_CLOCK_EXTERNAL_CRYSTAL_MASK | CPU_CLOCK_FAST_MASK) /* Clock generator mode */
#define CPU_CLOCK_VLP_CONFIG_1                             0U /* RUN power mode */

I've hand cranked these values for a 120MHz clock with a 16MHz crystal and they don't match the values above. Anyone know what these values should be given my scenario?

0 件の賞賛
返信
1 解決策
3,726件の閲覧回数
mjbcswitzerland
Specialist V

Ryan

There are two possibilities for configuring the K24 for 120MHz PLL operation from a 16 MHz crystal (120MHz core, 60MHz bus, 24MHz flash, 40MHz FlexBus clock [some bits are optional or flags and don't directly influencing the frequency]):
1:
MCG_C2 = 0xa4;
MCG_C5 = 0x23;
MCG_C6 = 0x46;
SIM_CLKDIV1 = 0x01240000
MCG_C1 = 0x28

2:
MCG_C2 = 0xa0;
MCG_C5 = 0x25;
MCG_C6 = 0x55;
SIM_CLKDIV1 = 0x01240000
MCG_C1 = 0x28

The values that you have for SIM_CLKDIV1 look suspect since they would give 30MHz Flash and 60MHz FlexClock, which are both out or spec for the K24. This makes me believe that the setup must be for a lower core clock speed (such as 96Mhz) where they would be just in spec.

Regards

Mark

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,726件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Ryan,

I copy the MCG diagram here. The external clock is 16MHz, the PLL input clock frequency range is limited from 2MHz to  4mHz, the VCOOUT clock frequency is from 48MHz to 120MHz, the VDIV is from 24 to 55.

The VCOOUT clock frequency=(external clock frequency)*VDIV/PRDIV.

If PRDIV=4, the PLL input clock frequency is 16MHz/4=4MHz. If the VDIV=30, the VCOOUT clock frequency is 16*30/4=120MHz.

If the PRDIV=8, the PLL input clock frequency is 16MHz/8=2MHz. If the VDIV=55, the VCOOUT clock frequency is 16*55/8=110MHz. Of course, this is not an option if you want to get 120MHz.

if PRDIV=6, VDIV=45, the VCOOUT frequency is 16MHz*45/6=120MHz, the PLL input frequency is 16MHz/6=2.66MHz, it is okay.

Mark gave the two MCG register configuration, pls follow up the state machine in the Figure 25-14. MCG mode state diagram to configure the MCG.

Hope it can help you.

BR

Xiangjun Rong

pastedImage_2.png

0 件の賞賛
返信
3,727件の閲覧回数
mjbcswitzerland
Specialist V

Ryan

There are two possibilities for configuring the K24 for 120MHz PLL operation from a 16 MHz crystal (120MHz core, 60MHz bus, 24MHz flash, 40MHz FlexBus clock [some bits are optional or flags and don't directly influencing the frequency]):
1:
MCG_C2 = 0xa4;
MCG_C5 = 0x23;
MCG_C6 = 0x46;
SIM_CLKDIV1 = 0x01240000
MCG_C1 = 0x28

2:
MCG_C2 = 0xa0;
MCG_C5 = 0x25;
MCG_C6 = 0x55;
SIM_CLKDIV1 = 0x01240000
MCG_C1 = 0x28

The values that you have for SIM_CLKDIV1 look suspect since they would give 30MHz Flash and 60MHz FlexClock, which are both out or spec for the K24. This makes me believe that the setup must be for a lower core clock speed (such as 96Mhz) where they would be just in spec.

Regards

Mark

0 件の賞賛
返信
3,726件の閲覧回数
ryanlush
Contributor IV

Well my 10ms delays are 12.5ms but my 20ms delays are 20ms so the 2.5ms must just be some RTOS overhead. More importantly I am able to clock the USB with the PLL now so I'm relatively confident my settings are correct. Thank you again Mark.

0 件の賞賛
返信
3,726件の閲覧回数
ryanlush
Contributor IV

These are the values I went with.

#define CPU_MCG_C1_CONFIG_0                                0x28U /* MCG_C1 */
#define CPU_MCG_C2_CONFIG_0                                0x24U /* MCG_C2 */
#define CPU_MCG_C4_CONFIG_0                                0x00U /* MCG_C4 */
#define CPU_MCG_C5_CONFIG_0                                0x23U /* MCG_C5 */
#define CPU_MCG_C6_CONFIG_0                                0x46U /* MCG_C6 */
#define CPU_MCG_SC_CONFIG_0                                0x02U /* MCG_SC */
#define CPU_OSC_CR_CONFIG_0                                0x80U /* OSC_CR */
#define CPU_SIM_SOPT1_CONFIG_0                             0x00080000UL /* SIM_SOPT1 */
#define CPU_SIM_SOPT2_CONFIG_0                             0x00010000UL /* SIM_SOPT2 */
#define CPU_SIM_CLKDIV1_CONFIG_0                           0x01240000UL /* SIM_CLKDIV1 */

The MCG status register reads 0x6E after the configuration but my 10ms delay is still 12.5ms.

0 件の賞賛
返信
3,726件の閲覧回数
ryanlush
Contributor IV

is it just PRDIV0 and VDIV0 that set the PLL frequency? Just changing the macros to Mark's values still doesn't give me the right frequency. I'm using MQX to generate a 10ms delay and toggle a pin so I wouldn't expect it to be a perfect 10ms pulse but it should be close. Maybe its just my systick that's wrong. I guess if I'm changing PLL frequency the systick reload value has to change too.

0 件の賞賛
返信