MQX 3.6.2 TAD (Task Aware Debugging) with Codewarrior CW 10 Special Edition

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MQX 3.6.2 TAD (Task Aware Debugging) with Codewarrior CW 10 Special Edition

跳至解决方案
3,375 次查看
juanee
Contributor III

Hello All,

 

I just installed Codewarrior 10, the special edition.  Is the TAD supported on this edition?

 

I searched the documentation for CW 10 and MQX 3.6.2 and I couldn’t find any information.

 

Thanks,

Juan

 

 ...

Codewarrior 10 Special Edition

Windows XP Pro

MQX 3.6.2

PEMicro USB ColdFire Multilink.

Custom Target based on Coldfire MCF52259.

0 项奖励
回复
1 解答
2,158 次查看
PetrL
NXP Employee
NXP Employee

Hi,

 

MQX TAD is available only for full Codewarrior version - Standard edition.

 

Regards,

PetrL

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,159 次查看
PetrL
NXP Employee
NXP Employee

Hi,

 

MQX TAD is available only for full Codewarrior version - Standard edition.

 

Regards,

PetrL

0 项奖励
回复
2,158 次查看
banjaxed
Contributor I

The whole area of CW and MQX is confusing enough without statements like this that are just downright WRONG.

 

Task-Aware Debugging is NOT available in the Standard Suite.

TAD is only available in the Professional Suite.

 

0 项奖励
回复
2,158 次查看
juanee
Contributor III

Thank you for your reply.

Juan

0 项奖励
回复