MCF52259 Tower with TWR-LCD and uGUI.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF52259 Tower with TWR-LCD and uGUI.

ソリューションへジャンプ
1,945件の閲覧回数
CarlFST60L
Senior Contributor II

Is there any plans to release the MCF52259 Tower working with TWR-LCD and eGUI instead of the JM128 /CN128? Is there any chance the TWR-LCD guys or MQX guys have a port to Coldfire V2 (52259) that I can use to get me started?

 

We bought the complete tower kit with TWR-LCD and MCF52259 module assuming that it would work 'out of the box' after seeing that MQX3.6.0 had eGUI support, instead, it requires the JM128 or CN128, and all its examples are to large for the demo version of Codewarrior 6.3 so its 'useless' to people with a Codewarrior 7.2 / Coldfire V2 license. We only have a license for CFV2 and the JM128/CN128 examples are to large for the free license, we are stuck.

0 件の賞賛
返信
1 解決策
1,196件の閲覧回数
CarlFST60L
Senior Contributor II

I think I have found the problem. I was working on the CD's that are shipped with the product, what you actually need to do is download the eGUI package from Freescale, the CD's are missing everything I was after.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,197件の閲覧回数
CarlFST60L
Senior Contributor II

I think I have found the problem. I was working on the CD's that are shipped with the product, what you actually need to do is download the eGUI package from Freescale, the CD's are missing everything I was after.

0 件の賞賛
返信