MCC library package

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCC library package

2,506件の閲覧回数
dry
Senior Contributor I

I'm trying to find where I can download MCC library package (for MQX) and embarrassingly I can't find it.

I can see it's included in the sources of MQX 4.2, but isn't there a stand-alone package downloadable package / installation archive?

Where can I find older versions of the library?  ( I tried a couple of older MQX installs, and did not find any .. :smileysad:)

4 返答(返信)

2,127件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello,

There is no a stand-alone package, MCC library is available after install MQX 4.0 or 4.1 or 4.2.

pastedImage_0.png

For more information about MCC programing, please check the below links:

Vybrid MCC User Guide For MCC Version 2.0 | Timesys Embedded Linux

https://community.freescale.com/docs/DOC-104422

I hope this helps


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,127件の閲覧回数
dry
Senior Contributor I

Thank you soledad for replying,

Yesterday before posting I tried MQX installs from  

DownloadsFile DescriptionFile Name
1Installer: FSLMQXOS_4_0_0_1_GAFSLMQXOS_4_0_0_1_GA.exe
DownloadsFile DescriptionFile Name
1Installer: MQX RTOS 4.1.2 for Vybrid Linux Base.gzMQX RTOS 4.1.2 for Vybrid Linux Base.gz.gz

Likely I'm taking wrong files, or i had some blindness but did not find any mcc folder in those.

Will retry taking just those Windows *.exe and install from them.

0 件の賞賛
返信

2,127件の閲覧回数
dry
Senior Contributor I

Sorry, correction to my original post.

I did find MCC there, but it was version 2.0

Now i found

Has MCC 1.2

And

Has 1.2 too.

Thanks soledad.

Was MCC ver 1.2 last version from ver 1.x series?

0 件の賞賛
返信

2,127件の閲覧回数
soledad
NXP Employee
NXP Employee

For MQX 4.2 the MCC ver is 2.1.

Regards

Sol

0 件の賞賛
返信