LPUART support in MQX for K65

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPUART support in MQX for K65

1,330件の閲覧回数
yossisarusi
Contributor I

Can not see the support of the LPUART in the MQX 4_2. 

Do I miss something.

Thanks

0 件の賞賛
返信
1 返信

1,182件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Yosef Sarusi

     LPUART is supported in MQX 5.1. But it is under commercial license. Please check the following link for more details.

https://www.nxp.com/docs/en/release-note/MQXRN.pdf 

MQX™ v5 Software Solutions|NXP 

If you want to use MQX 4.2 with lpuart, I would suggest you make it by yourself. It is possible to merger a bare metal driver into MQX, however you need to take care about the hardware initialization, some hardware is already initialized in BSP code therefore cannot copy-paste your bare mental code.

You also can refer to lpuart driver in KSDK package, and port it to MQX 4.2.

Regards

Daniel



-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信