K65-TWR 180MHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K65-TWR 180MHz

1,505件の閲覧回数
Mike_d
Contributor IV

Hi,

What changes do I need to make to the BSP files to run the K65 at 180MHz?

Thanks,

-Mike

0 件の賞賛
返信
2 返答(返信)

1,361件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi  Michael del Busto

TWR_K65F180M is already supported in classic MQX 4.2, please check the following folder.

Freescale_MQX_4_2\mqx\source\bsp\twrk65f180m


Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,361件の閲覧回数
Mike_d
Contributor IV

Hi Daniel,

The initialization files run the K65 at 120MHz.  I would like to know what changes to make to run at 180MHz.  These files appear to be generated by processor expert but I cannot create a PE project for the K65.

Regards,

-Mike 

0 件の賞賛
返信