K22FX512 base BSP MQX 4.2 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K22FX512 base BSP MQX 4.2 ?

1,237件の閲覧回数
cavebiker
Contributor V

I started a project using a K20FX512. The base BSP I used in MQX 4.2 was the twrk60f120m BSP. 

I need lower power so attempting to use a K22FX512 part, it has the same footprint. All good.

My question is what is the base BSP in MQX 4.2 I need to start with, and or is there any BSP in MQX 4.2 for this part?

Thank you in advance for any help.

Cheers,

Tom

0 件の賞賛
返信
1 返信

1,151件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

The closest MQX BSP Board is the TWR-K21F120M


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信