Is it possible to use DMA with the MFS in MQX RTOS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to use DMA with the MFS in MQX RTOS?

1,245件の閲覧回数
naftalir
Contributor III

Hi,

 

I am using the MQX RTOS with MFS and want to write to SD-Card with the help of DMA, so the CPU wont be busy with the writing operation.

Is it possible?

 

 

 

Thank you in advance,

Naftali.

0 件の賞賛
返信
2 返答(返信)

871件の閲覧回数
pavel_chromy
NXP Employee
NXP Employee

I am afraid that it is not possible to use DMA for SDCARD (neither SPI nor eSDHC mode) so far.

DMA support is on the schedule so it will be included in future release of MQX.

0 件の賞賛
返信

871件の閲覧回数
naftalir
Contributor III

Hi Pavel,

i ran some tests in mqx 4.0 and it seems that the write speed on SDHC cards are the same as 3.8.1.

is the improvement of speed suppose to be in this release or the next one (MQX 4.1)?

and does the DMA will be used too in the next release?

Best regards,

Naftali.

0 件の賞賛
返信