IEEE1588 Stack on KSDK 1.2/1.3?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IEEE1588 Stack on KSDK 1.2/1.3?

831件の閲覧回数
joseraffucci
Contributor IV

I am evaluating the 1588 functionality on the K64 processor for an upcoming project.  I have been able to get the sample 1588 code for MQX 4.2 up and running on both FRDMK64F and a TWRK64F boards.  Unfortunately, that's as far as I've been able to get as we are working with KDSK1.2 (and maybe 1.3 shortly).   I spent a little time trying to see the scope of porting the mqx1588 project myself and ran into a few roadblocks -- mostly the lack of a macnet driver in ksdk.  It's possible that some of the 1588 functionality has been rolled into the enet driver, I just haven't stared at it enough so see it.

Can someone tell me if a 1588 port is forthcoming, hopefully with an ETA?  I would hate to go any further down this rabbit hole only to find that there's a FS engineer working on it.

0 件の賞賛
返信
0 返答(返信)