- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I've been using a K64 Tower Board with CW 10.6 and MQX 4.1. Please bare with me as I try to explain what I'm trying to accomplish.
1. The MQX 4.1 SPI driver has "SPI0_SIN" on PTD3 / "SPI0_SOUT" on PTD2 / "SPI0_SCK" on PTD1 , (I have verified this stuff with a scope using a provided example project)
2. According to the data sheet of the K64, SPI0_SIN/SPI0_SOUT/SPI0_SCK can be "routed" to different pins, for example SPI0_SIN can also be "routed" to PTA17, PTC7 (in addition to PTD3 (which is the default))
3. MY QUESTION IS: How can I change the default "pin mapping" ? For example how can I make SPI0_SIN be "routed" to PTA17 as opposed to PTD3 ?
Thank you for your time and help in advance,
Gino
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
You need to modify three files:
- User_config.h : This is in order to enable the SPI driver
#define BSPCFG_ENABLE_SPI0 1
2. twrk64f120m.h : You need to modify the below parameters according your needs
/*-----------------------------------------------------------------------------
** DSPI
*/
#define BSP_DSPI_INT_LEVEL (4)
#define BSP_SPI_MEMORY_CHANNEL (0)
#define BSP_DSPI0_DMA_RX_CHANNEL (0)
#define BSP_DSPI0_DMA_TX_CHANNEL (1)
#define BSP_DSPI0_DMA_RX_SOURCE (14)
#define BSP_DSPI0_DMA_TX_SOURCE (15)
#define BSP_DSPI1_DMA_RX_CHANNEL (2)
#define BSP_DSPI1_DMA_TX_CHANNEL (3)
#define BSP_DSPI1_DMA_RX_SOURCE (16)
#define BSP_DSPI1_DMA_TX_SOURCE (16)
#define BSP_DSPI2_DMA_RX_CHANNEL (4)
#define BSP_DSPI2_DMA_TX_CHANNEL (5)
#define BSP_DSPI2_DMA_RX_SOURCE (17)
#define BSP_DSPI2_DMA_TX_SOURCE (17)
3. init_gpio.h : Also you need to modify the below parameters according your needs
/*FUNCTION*-------------------------------------------------------------------
*
* Function Name : _bsp_dspi_io_init
* Returned Value : MQX_OK or -1
* Comments :
* This function performs BSP-specific initialization related to DSPI
*
*END*----------------------------------------------------------------------*/
_mqx_int _bsp_dspi_io_init
(
uint32_t dev_num
)
{
SIM_MemMapPtr sim = SIM_BASE_PTR;
PORT_MemMapPtr pctl;
switch (dev_num)
{
case 0:
/* Configure GPIOE for DSPI0 peripheral function */
pctl = (PORT_MemMapPtr)PORTE_BASE_PTR;
pctl->PCR[16] = PORT_PCR_MUX(2); /* DSPI0.PCS0 */
pctl->PCR[17] = PORT_PCR_MUX(2); /* DSPI0.SCK */
pctl->PCR[18] = PORT_PCR_MUX(2); /* DSPI0.SOUT */
pctl->PCR[19] = PORT_PCR_MUX(2); /* DSPI0.SIN */
/* Enable clock gate to DSPI0 module */
sim->SCGC6 |= SIM_SCGC6_DSPI0_MASK;
break;
case 1:
/* Configure GPIOE for DSPI1 peripheral function */
pctl = (PORT_MemMapPtr)PORTE_BASE_PTR;
pctl->PCR[1] = PORT_PCR_MUX(2); /* DSPI1.SOUT */
pctl->PCR[2] = PORT_PCR_MUX(2); /* DSPI1.SCK */
pctl->PCR[3] = PORT_PCR_MUX(2); /* DSPI1.SIN */
pctl->PCR[4] = PORT_PCR_MUX(2); /* DSPI1.PCS0 */
/* Enable clock gate to DSPI1 module */
sim->SCGC6 |= SIM_SCGC6_DSPI1_MASK;
break;
case 2:
/* Configure GPIOD for DSPI2 peripheral function */
pctl = (PORT_MemMapPtr)PORTD_BASE_PTR;
pctl->PCR[11] = PORT_PCR_MUX(2); /* DSPI2.PCS0 */
pctl->PCR[12] = PORT_PCR_MUX(2); /* DSPI2.SCK */
pctl->PCR[13] = PORT_PCR_MUX(2); /* DSPI2.SOUT */
pctl->PCR[14] = PORT_PCR_MUX(2); /* DSPI2.SIN */
pctl->PCR[15] = PORT_PCR_MUX(2); /* DSPI2.PCS1 */
/* Enable clock gate to DSPI2 module */
sim->SCGC3 |= SIM_SCGC3_DSPI2_MASK;
break;
default:
/* do nothing if bad dev_num was selected */
return -1;
}
return MQX_OK;
}
You can find these files at the path C:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk64f120m
Don’t forget to rebuild the libraries after these modifications.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello - What do the numbers represent (4,5,17,17) ?
Thanks,
Louie
#define BSP_DSPI2_DMA_RX_CHANNEL (4)
#define BSP_DSPI2_DMA_TX_CHANNEL (5)
#define BSP_DSPI2_DMA_RX_SOURCE (17)
#define BSP_DSPI2_DMA_TX_SOURCE (17)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
You need to modify three files:
- User_config.h : This is in order to enable the SPI driver
#define BSPCFG_ENABLE_SPI0 1
2. twrk64f120m.h : You need to modify the below parameters according your needs
/*-----------------------------------------------------------------------------
** DSPI
*/
#define BSP_DSPI_INT_LEVEL (4)
#define BSP_SPI_MEMORY_CHANNEL (0)
#define BSP_DSPI0_DMA_RX_CHANNEL (0)
#define BSP_DSPI0_DMA_TX_CHANNEL (1)
#define BSP_DSPI0_DMA_RX_SOURCE (14)
#define BSP_DSPI0_DMA_TX_SOURCE (15)
#define BSP_DSPI1_DMA_RX_CHANNEL (2)
#define BSP_DSPI1_DMA_TX_CHANNEL (3)
#define BSP_DSPI1_DMA_RX_SOURCE (16)
#define BSP_DSPI1_DMA_TX_SOURCE (16)
#define BSP_DSPI2_DMA_RX_CHANNEL (4)
#define BSP_DSPI2_DMA_TX_CHANNEL (5)
#define BSP_DSPI2_DMA_RX_SOURCE (17)
#define BSP_DSPI2_DMA_TX_SOURCE (17)
3. init_gpio.h : Also you need to modify the below parameters according your needs
/*FUNCTION*-------------------------------------------------------------------
*
* Function Name : _bsp_dspi_io_init
* Returned Value : MQX_OK or -1
* Comments :
* This function performs BSP-specific initialization related to DSPI
*
*END*----------------------------------------------------------------------*/
_mqx_int _bsp_dspi_io_init
(
uint32_t dev_num
)
{
SIM_MemMapPtr sim = SIM_BASE_PTR;
PORT_MemMapPtr pctl;
switch (dev_num)
{
case 0:
/* Configure GPIOE for DSPI0 peripheral function */
pctl = (PORT_MemMapPtr)PORTE_BASE_PTR;
pctl->PCR[16] = PORT_PCR_MUX(2); /* DSPI0.PCS0 */
pctl->PCR[17] = PORT_PCR_MUX(2); /* DSPI0.SCK */
pctl->PCR[18] = PORT_PCR_MUX(2); /* DSPI0.SOUT */
pctl->PCR[19] = PORT_PCR_MUX(2); /* DSPI0.SIN */
/* Enable clock gate to DSPI0 module */
sim->SCGC6 |= SIM_SCGC6_DSPI0_MASK;
break;
case 1:
/* Configure GPIOE for DSPI1 peripheral function */
pctl = (PORT_MemMapPtr)PORTE_BASE_PTR;
pctl->PCR[1] = PORT_PCR_MUX(2); /* DSPI1.SOUT */
pctl->PCR[2] = PORT_PCR_MUX(2); /* DSPI1.SCK */
pctl->PCR[3] = PORT_PCR_MUX(2); /* DSPI1.SIN */
pctl->PCR[4] = PORT_PCR_MUX(2); /* DSPI1.PCS0 */
/* Enable clock gate to DSPI1 module */
sim->SCGC6 |= SIM_SCGC6_DSPI1_MASK;
break;
case 2:
/* Configure GPIOD for DSPI2 peripheral function */
pctl = (PORT_MemMapPtr)PORTD_BASE_PTR;
pctl->PCR[11] = PORT_PCR_MUX(2); /* DSPI2.PCS0 */
pctl->PCR[12] = PORT_PCR_MUX(2); /* DSPI2.SCK */
pctl->PCR[13] = PORT_PCR_MUX(2); /* DSPI2.SOUT */
pctl->PCR[14] = PORT_PCR_MUX(2); /* DSPI2.SIN */
pctl->PCR[15] = PORT_PCR_MUX(2); /* DSPI2.PCS1 */
/* Enable clock gate to DSPI2 module */
sim->SCGC3 |= SIM_SCGC3_DSPI2_MASK;
break;
default:
/* do nothing if bad dev_num was selected */
return -1;
}
return MQX_OK;
}
You can find these files at the path C:\Freescale\Freescale_MQX_4_1\mqx\source\bsp\twrk64f120m
Don’t forget to rebuild the libraries after these modifications.
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank you, that worked