HTTP post

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HTTP post

2,093 Views
Swapnil_Enable
Contributor III

Hi i am trying to POST data to Google spreadsheet like andrino, but i am not able succeed. i have return the code for POST.

strcat (cServer_WriteBuff,"entry.1446189103=");
strcat (cServer_WriteBuff,POST);
strcat (cServer_WriteBuff,"&submit=Submit");
value = strlen(cServer_WriteBuff);
error = send(sock, "POST /formResponse?formkey=", sizeof("POST /formResponse?formkey="), 0);
error = send(sock, (void *)formkey, sizeof(formkey), 0);
error = send(sock, "&ifq HTTP/1.1\r\n", sizeof("&ifq HTTP/1.1\r\n"), 0);
error = send(sock, "Host: spreadsheets.google.com\r\n", sizeof("Host: spreadsheets.google.com\r\n"), 0);
error = send(sock, "Content-Type: application/x-www-form-urlencoded\r\n", sizeof("Content-Type: application/x-www-form-urlencoded\r\n"), 0);
error = send(sock, "Connection: close\r\n", sizeof("Connection: close\r\n"), 0);
error = send(sock, (void *)value, sizeof(value), 0);
error = send(sock, "\r\n", sizeof("\r\n"), 0);
error = send(sock, "\r\n", sizeof("\r\n"), 0);
error = send(sock, (void *)cServer_WriteBuff, sizeof(cServer_WriteBuff), 0);
error = send(sock, "\r\n", sizeof("\r\n"), 0);
error = send(sock, "\r\n", sizeof("\r\n"), 0);

  but when i check it on Hercules terminal, it only shows " POST /formResponse?formkey=" can anyone please help to figure out, or any suggestion. i am tring to use httpsrv code but being a beginner not able to figure how to use it.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,614 Views
karelm_
Contributor IV

Hi,

please try to use function strlen instead of sizeof in calls of send() function. Using sizeof in this context means that you also send terminating null character ('\0') in your messages, which is probably why you cannot receive any other than first message. Also on line 16 you are calling sizeof(formkey). I assume, that variable formkey is pointer so sizeof will return 4, which is probably not what you want. If you want to get length of string formkey is pointing to you should use strlen(formkey).

Best regards

Karel

0 Kudos
Reply