The message you are trying to access is permanently deleted.
Hello
To upgrade and add some function to an existing product, I would know if with MQX 4.2 (on a Kinetis K70) we can use an HTTP Client?
The aim for us is to send a couple of data to a HTTp server.
Regards,
Solved! Go to Solution.
Hi @arnogir :
Please refer to attached zip file.
Regards
Daniel
View solution in original post
Hello,
In the same way, if MQX can integrate a FTP client? (To send file to a distant FTP server)?
Is there an exemple?
Thank
Hi
I would suggest you refer to AN4417. It demonstrated http client implementation using MQX RTOS capabilities. The hardware used to illustrate this is the TWR-K60N512.
Thank a lot.
Could you indicate me where can I find the .zip which contains file exemple?
Are link from "Frescale" are broken.
Thank a lot
In the same way, is the HTTPS is possible?
Yes, the link is broken. I can not get it neither.
I will update you if I get it.