FRDMK64 BOOTLOADER

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDMK64 BOOTLOADER

1,483 Views
sudhakarp
Contributor V

hI,

     I want bootloader code for custom board. i am using frdmk64f120 controller, kds 2.0 and KSDK 1.1.0. in my custom board

am not using OPENSDA chip. so i want sample bootloader code. using external data flash am going to update my Application code.

so i need your support to implement this one. can you give any sample bootloader code working with KDS IDE.

thanks and regards,

sudhakar p

0 Kudos
Reply
1 Reply

1,060 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello sudhakar p:

For loading the firmware from an external memory unfortunately there is no example available for K64.

Basically you need at least 2 things: external flash driver + internal flash routines.

- You need to implement the external memory driver.

- For the flash routines you can take the driver C90TFS integrated with KSDK: C:\Freescale\KSDK_1.2.0\platform\drivers\src\flash\C90TFS

For other bootloader interfaces (e.g. UART, USB HID), you can download Kinetis Bootloader (KBOOT):

Kinetis Bootloader|Freescale

This includes a KDS project for K64.

There are other examples about bootloader implementations for your reference, such as AN2295 (UART bootloader):

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf

Regards!

Jorge Gonzalez

0 Kudos
Reply