Error: Couldn't download flash driver file. Flash Driver is Not Linked To Zero.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error: Couldn't download flash driver file. Flash Driver is Not Linked To Zero.

1,358 Views
danielchai
Senior Contributor I

Hi,

I am tring to download the httpsrv project to TWRK60F120 board using CW10.4, MQX4.0.1.

But it gives me some errrors: Error:  Couldn't download flash driver file.  Flash Driver is Not Linked To Zero.

I did it step by step just as shown below. Any suggestions or ideas will be appreciated.

1. 1.png

2. 2.png

3. 3.png

0 Kudos
Reply
2 Replies

957 Views
DavidS
NXP Employee
NXP Employee

Hi Daniel,

Please open the *.ttf file and change the Target RAM Address: from 0x20000000 to 0x1fff00000..

Below is picture of my script setup and I just verified that it runs on TWR-K60F120M.

ScreenHunter_42 Nov. 01 15.24.gif

Regards,

David
PS

I've attached the script file too.

0 Kudos
Reply

957 Views
danielchai
Senior Contributor I

Hi David,

Thank you.

Now it can download the code but during downloading, it has other error:

Error:  Erase failed.   Flash driver reports the following error(s):  Chip reported error during program. Please check that the sector you are programming is erased.

Untitled.png

Thank you.

-Daniel

0 Kudos
Reply