Debug trouble

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug trouble

2,222 Views
jonnyescobar
Contributor II

hi

I am triying to debug my program, this stop on ldr r0, there is a discussion but the link doesn't work

Thread [1] <main> (Suspended : Signal : SIGTRAP:Trace/breakpoint trap)

__boot() at boot.S:66 0x7cc

the code where happen is:

/* Disable interrupts and clear pending flags */

        ldr r0, =NVIC_ICER0

        ldr r1, =NVIC_ICPR0

        ldr r2, =0xFFFFFFFF

        mov r3, #8

thanks a lot

0 Kudos
Reply
4 Replies

1,997 Views
soledad
NXP Employee
NXP Employee

Did you refer to this link KDS and PE Micro Debugger Setup?  ???

Regards

Sol

0 Kudos
Reply

1,997 Views
jonnyescobar
Contributor II

Hello

I am using MQX,  k64FN1M0VLQ12 and KDS 3.0, my board was worrking but i did minor changes on Processor Expert GPIO configuration.

Thanks

0 Kudos
Reply

1,997 Views
soledad
NXP Employee
NXP Employee

Hello Jonny,

Please check the link below and let me know if this helps.

KDS and PE Micro Debugger Setup? 

Regards

Sol

0 Kudos
Reply

1,997 Views
soledad
NXP Employee
NXP Employee

Hello Jonny,

Are you using MQX??

Which device are you using??

Which IDE are you using?

Regards

Sol

0 Kudos
Reply