DDR3 Timing Using Vybrid with MQX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DDR3 Timing Using Vybrid with MQX

1,180 次查看
olafschulz
Contributor I

​cCustomer Use a Vybrid Professor with DDR3 Typ K4B1G1646G-BCH9. What are the best initial Values in Timing when using MQX, are the Setting in Freescale_MQX_4_2\mqx\source\bsp\twrvf65gs10_a5\init_hw.c the best or a good startpoint.

0 项奖励
回复
1 回复

1,064 次查看
b36401
NXP Employee
NXP Employee

There is nothing special with timing for MQX.

You can use those timing values as well.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复