Configuring RTCS to have less protocols

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuring RTCS to have less protocols

2,778件の閲覧回数
Ardoster
Contributor III

Hi

 

I'm trying to reduce the space memory of my RTCS code. Right now, I'm trying to rebuild manually all my RTCS library, but I'm not very sure this is the correct way to remove protocols or application from my library because this way is very difficult to do without errors. Is there another simplier way to make RTCS take less space memory? Pherhaps editing a .h file, modifying includes, etc?

 

Thanks you in advance, and very good weekend.

 

Regards

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,568件の閲覧回数
Ardoster
Contributor III
Any idea?
0 件の賞賛
返信

1,568件の閲覧回数
flashtoo
Contributor I

I think you can just set them to 0 in your user_config.h file. I beleive the linker is smart enought not to link them in if not needed but I have not tested this.

0 件の賞賛
返信