Code Warrior Library Project in MQX 4.2?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code Warrior Library Project in MQX 4.2?

1,251件の閲覧回数
erictexley
Contributor I

In MQX4.1 there was a library project for CodeWarrior 10.x which would set up all the projects required to build MQX.   Does that project file exist in MQX4.2?  I don't see it

0 件の賞賛
返信
1 返信

1,143件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Eric Texley

The library project files are in the relative build folders.

Let's take frdmK64f for example, the libraries are in the following folders

Freescale_MQX_4_2\mqx\build\cw10gcc\bsp_frdmk64f

Freescale_MQX_4_2\mqx\build\cw10gcc\psp_frdmk64f

Freescale_MQX_4_2\rtcs\build\cw10gcc\rtcs_frdmk64f

Freescale_MQX_4_2\mfs\build\cw10gcc\mfs_frdmk64f

I hope it helps

Have a great day!

Regards

Daniel

-----------------------------------------------------------------------------------------------------------

If this post answered your question, please click correct or helpful, thank you

0 件の賞賛
返信