Code Warrior Library Project in MQX 4.2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warrior Library Project in MQX 4.2?

1,260 Views
erictexley
Contributor I

In MQX4.1 there was a library project for CodeWarrior 10.x which would set up all the projects required to build MQX.   Does that project file exist in MQX4.2?  I don't see it

0 Kudos
Reply
1 Reply

1,152 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Eric Texley

The library project files are in the relative build folders.

Let's take frdmK64f for example, the libraries are in the following folders

Freescale_MQX_4_2\mqx\build\cw10gcc\bsp_frdmk64f

Freescale_MQX_4_2\mqx\build\cw10gcc\psp_frdmk64f

Freescale_MQX_4_2\rtcs\build\cw10gcc\rtcs_frdmk64f

Freescale_MQX_4_2\mfs\build\cw10gcc\mfs_frdmk64f

I hope it helps

Have a great day!

Regards

Daniel

-----------------------------------------------------------------------------------------------------------

If this post answered your question, please click correct or helpful, thank you

0 Kudos
Reply