Can the unit of Task time slice be changed?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can the unit of Task time slice be changed?

ソリューションへジャンプ
4,346件の閲覧回数
george
Senior Contributor II

Hi all,

I'm using MQX 3.8.1 on TWR-K60N512.

And, the scheduling of MQX Task uses Round robin.

I want to set the Time slice of Tasks to 100uSec.

Is the setting possible?

If possible, please tell me the way.

Best regards,

George

タグ(5)
1 解決策
3,674件の閲覧回数
JuroV
NXP Employee
NXP Employee

Hello,

the default time slice unit is number of ticks. Ticks are set by the frequency of the system timer in the <board>.h file.

元の投稿で解決策を見る

7 返答(返信)
3,674件の閲覧回数
Swapnil_Enable
Contributor III

u can set it by changing the Task Templete. Please refer 3.2.20 in MQXRM pdf or 3.2.2 in MQXUG.pdf.

location would be C:\Program Files\Freescale\Freescale MQX 3.8\doc\mqx

ex:

{INIT_TASK,        init_Task,      800,   9,  "initTask",  MQX_AUTO_START_TASK, 0, 100},

the bold on will change the time slice of task.

0 件の賞賛
返信
3,674件の閲覧回数
george
Senior Contributor II

Hi Katre,

In my understanding, The default time unit of slice is milliseconds.

I want to set time slice fewer than the minimum which can set it.

Plase tell me how to change to microsec from millisec.

Best Regards,

George

0 件の賞賛
返信
3,675件の閲覧回数
JuroV
NXP Employee
NXP Employee

Hello,

the default time slice unit is number of ticks. Ticks are set by the frequency of the system timer in the <board>.h file.

3,674件の閲覧回数
Swapnil_Enable
Contributor III

Thanks Juraj, George i to agree with him, as per my knowledge....the time setting works on ticks so u can make it to microsec....u need to do some calculation to get ur desired number

0 件の賞賛
返信
3,674件の閲覧回数
george
Senior Contributor II

Thanks Juraj and Swapnil,

Is the parameter which you say the following?

  #ifndef BSP_ALARM_FREQUENCY

      #define BSP_ALARM_FREQUENCY             (200)

  #endif

Is my understanding correct?

Best Regards,

George

0 件の賞賛
返信
3,674件の閲覧回数
JuroV
NXP Employee
NXP Employee

Yes, that's the parameter.

0 件の賞賛
返信
3,674件の閲覧回数
george
Senior Contributor II

Thanks Juraj,

0 件の賞賛
返信