Can the unit of Task time slice be changed?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the unit of Task time slice be changed?

Jump to solution
2,831 Views
george
Senior Contributor II

Hi all,

I'm using MQX 3.8.1 on TWR-K60N512.

And, the scheduling of MQX Task uses Round robin.

I want to set the Time slice of Tasks to 100uSec.

Is the setting possible?

If possible, please tell me the way.

Best regards,

George

1 Solution
2,159 Views
JuroV
NXP Employee
NXP Employee

Hello,

the default time slice unit is number of ticks. Ticks are set by the frequency of the system timer in the <board>.h file.

View solution in original post

7 Replies
2,159 Views
Swapnil_Enable
Contributor III

u can set it by changing the Task Templete. Please refer 3.2.20 in MQXRM pdf or 3.2.2 in MQXUG.pdf.

location would be C:\Program Files\Freescale\Freescale MQX 3.8\doc\mqx

ex:

{INIT_TASK,        init_Task,      800,   9,  "initTask",  MQX_AUTO_START_TASK, 0, 100},

the bold on will change the time slice of task.

0 Kudos
Reply
2,159 Views
george
Senior Contributor II

Hi Katre,

In my understanding, The default time unit of slice is milliseconds.

I want to set time slice fewer than the minimum which can set it.

Plase tell me how to change to microsec from millisec.

Best Regards,

George

0 Kudos
Reply
2,160 Views
JuroV
NXP Employee
NXP Employee

Hello,

the default time slice unit is number of ticks. Ticks are set by the frequency of the system timer in the <board>.h file.

2,159 Views
Swapnil_Enable
Contributor III

Thanks Juraj, George i to agree with him, as per my knowledge....the time setting works on ticks so u can make it to microsec....u need to do some calculation to get ur desired number

0 Kudos
Reply
2,159 Views
george
Senior Contributor II

Thanks Juraj and Swapnil,

Is the parameter which you say the following?

  #ifndef BSP_ALARM_FREQUENCY

      #define BSP_ALARM_FREQUENCY             (200)

  #endif

Is my understanding correct?

Best Regards,

George

0 Kudos
Reply
2,159 Views
JuroV
NXP Employee
NXP Employee

Yes, that's the parameter.

0 Kudos
Reply
2,159 Views
george
Senior Contributor II

Thanks Juraj,

0 Kudos
Reply