Can the MQX USB device and host stacks work at the same time?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the MQX USB device and host stacks work at the same time?

1,157 Views
fenz
Contributor II

Hi,

 

We are using a MCF5329 which has a dedicated USB host hardware and a USB dual role hardware (that can be configured to act as a host/device/OTG).

 

From a hw perspecitive it seems to me that the chip can act as both a host and device at the same time.

 

The question is whether the Host and Device sw stacks can coexist and work independently at the same time?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

656 Views
JuroV
NXP Employee
NXP Employee

Unfortunatelly, they cannot at this moment from various reasons.

0 Kudos
Reply