Bug report: Memory overflow in ifdns

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bug report: Memory overflow in ifdns

1,585件の閲覧回数
chrissolomon
Contributor III

Hi,

In MQX 4.0.1 (possibly later, haven't checked) there is an off by one error in rtcs/source/if/ifdns.c, in the function DNS_insert_slist_entry.

Original code snippit:

(starts at line 254)

      if (usr_slist_entry_ptr->NAME_PTR)

      {

         tmp_str = RTCS_mem_alloc_system( strlen(usr_slist_entry_ptr->NAME_PTR) );

         if (tmp_str == NULL)

            return RTCSERR_DNS_UNABLE_TO_ALLOCATE_MEMORY;

         strcpy(tmp_str, usr_slist_entry_ptr->NAME_PTR);

      }

The problem is strlen gives the length of the string NOT INCLUDING THE NULL TERMINATION, where as strcpy copies including the null termination.

My fix:

      if (usr_slist_entry_ptr->NAME_PTR)

      {

         tmp_str = RTCS_mem_alloc_system( strlen(usr_slist_entry_ptr->NAME_PTR) + 1 );

         if (tmp_str == NULL)

            return RTCSERR_DNS_UNABLE_TO_ALLOCATE_MEMORY;

         strcpy(tmp_str, usr_slist_entry_ptr->NAME_PTR);

      }

It's a simple fix, and for the most part it wont cause any problem, unless the string length happens to fit in the allocation block perfectly, then the first byte of the next blocks header will be zeroed, with unpredictable results.

ラベル(1)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,417件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

The DNS system has been re-written for MQX 4.2, Next MQX release won't have that source files at all. Thank you

0 件の賞賛
返信

1,417件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

Thank you for reporting this, I will forward your post to software team.


Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信