BSP cloning wizard for KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BSP cloning wizard for KDS

Jump to solution
3,756 Views
lvw
Contributor II

I am currently testing KDS + MQX.

MQX comes with KDS ready libraries for many evaluation boards. But the cloning wizard is missing the KDS IDE target, making difficult to port it on my own prototype board.

The 'Convert CodeWarrior project' option in KDS is not reacting on MQX libraries projects (nothing happens).

It would be very nice if some tool was available.

1 Solution
3,198 Views
RadekS
NXP Employee
NXP Employee

I would like to apologize. I forget update this thread.

Yes, KDS support was added into Freescale MQX RTOS 4.1.1 Cloning Wizard Patch https://www.freescale.com/webapp/sps/download/license.jsp?colCode=FSLMQXCW_4_1_1_OS

Released: 10/24/2014

View solution in original post

0 Kudos
Reply
4 Replies
3,198 Views
RadekS
NXP Employee
NXP Employee

Thank you for your report.

We are working on that and it will be fixed in near feature. We have to fix BSPCloningWizard application for that.

We will probably release patch for BSPCloningWizard independently on MQX updates.

I will update this thread when patch will be available.


Have a great day,
RadekS

0 Kudos
Reply
3,198 Views
ebee
Contributor II

RadekS,

Is there any update on this yet as I am looking to port the MQX to our new products using the KDS.

Thanks Ian

0 Kudos
Reply
3,199 Views
RadekS
NXP Employee
NXP Employee

I would like to apologize. I forget update this thread.

Yes, KDS support was added into Freescale MQX RTOS 4.1.1 Cloning Wizard Patch https://www.freescale.com/webapp/sps/download/license.jsp?colCode=FSLMQXCW_4_1_1_OS

Released: 10/24/2014

0 Kudos
Reply
3,198 Views
lvw
Contributor II

Thank you very much Radeks, for the good news.

Luc

0 Kudos
Reply