ADC Bug found in TWRK60f120M ini_gpio.c

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC Bug found in TWRK60f120M ini_gpio.c

1,021件の閲覧回数
keithtang
Contributor IV

I am new in MQX, and still learning how to use MQX on TWRK60F120M board. Through scanning the files, I found one bug, which I hope someone can verify it.

 

In init_gpio.c, line 456:

 

        case ADC_SOURCE_MODULE(1): /* ADC0 */
            if (ADC_GET_MUXSEL(source) == ADC_SOURCE_MUXSEL_A)
            {
                if(ch < 4)
                {
                    gpio_port = adc0_conv_table_a[ch - 4];
                }
                else
                {
                    return IO_ERROR; /* channel does not exist */
                }
            }

 

Obviously if ch < 4, ch-4 will be negative. I believe it should be:

 

        case ADC_SOURCE_MODULE(1): /* ADC0 */
            if (ADC_GET_MUXSEL(source) == ADC_SOURCE_MUXSEL_A)
            {
                if(ch >= 4 && ch <= 7)
                {
                    gpio_port = adc0_conv_table_a[ch - 4];
                }
                else
                {
                    return IO_ERROR; /* channel does not exist */
                }
            }

 

or we can inert the code:

 

        case ADC_SOURCE_MODULE(1): /* ADC0 */
            if (ADC_GET_MUXSEL(source) == ADC_SOURCE_MUXSEL_A)
            {
                if(ch < 4 || ch > 7)
                {
                    return IO_ERROR; /* channel does not exist */
                }
                else
                {
                    gpio_port = adc0_conv_table_a[ch - 4];
                }
            }

 

Please let me know if this is the case. Thanks.

0 件の賞賛
返信
2 返答(返信)

767件の閲覧回数
c0170
Senior Contributor III

Hello,

 

I am going to reply to every single thread you created.

The last two solutions could be used in this case. It's been reported and we are going to correct this error in the init configuration.

 

 

Regards,

MartinK

 

0 件の賞賛
返信

767件の閲覧回数
keithtang
Contributor IV

Thanks MartinK.

 

I just revisit the files, and found that the above solutions were conceptually right but practically incorrect, and I have fixed them.

 

For those who cannot wait for the new release, here is what I have done to get it work:

 

1. In ".\Freescale MQX 3.8\mqx\source\io\adc\adc_mk60.h":

 

Modify this line so that it looks like this:

#define ADC1_SOURCE_AD20        (ADC_SOURCE_MODULE(2) | ADC_SOURCE_MUXSEL_B | ADC_SOURCE_CHANNEL(20))

 

Insert this line:

#define ADC1_SOURCE_DM1             (ADC1_SOURCE_AD20)

 

2. In ".\Freescale MQX 3.8\mqx\source\bsp\twrk60f120m\twrk60f120m.h":

 

Modify this line:

#define BSP_ADC_CH_POT                  (ADC1_SOURCE_DM1)

 

3. In ".\Freescale MQX 3.8\mqx\source\bsp\twrk60f120m\init_gpio.c":

 

Modify so that it looks like this:

    const static uint_8 adc1_conv_table_bx[] = {
        ADC_SIG_NC,         /* 0 leave as default */
        ADC_SIG_NC,         /* 1 leave as default */
        ADC_SIG_NC,         /* 2 leave as default */
        ADC_SIG_NC,         /* 3 leave as default */
        ADC_SIG_PORTC | 8,  /* ADC1_SE4b/CMP0_IN2 */
        ADC_SIG_PORTC | 9,  /* ADC1_SE5b/CMP0_IN3 */
        ADC_SIG_PORTC | 10, /* ADC1_SE6b */
        ADC_SIG_PORTC | 11, /* ADC1_SE7b */
        ADC_SIG_PORTB | 0,  /* ADC0_SE8/ADC1_SE8/ADC2_SE8/ADC3_SE8/TSI0_CH0 */
        ADC_SIG_PORTB | 1,  /* ADC0_SE9/ADC1_SE9/ADC2_SE9/ADC3_SE9/TSI0_CH6 */
        ADC_SIG_PORTB | 4,  /* ADC1_SE10 */
        ADC_SIG_PORTB | 5,  /* ADC1_SE11 */
        ADC_SIG_PORTB | 6,  /* ADC1_SE12 */
        ADC_SIG_PORTB | 7,  /* ADC1_SE13 */
        ADC_SIG_PORTB | 10, /* ADC1_SE14 */
        ADC_SIG_PORTB | 11, /* ADC1_SE15 */
        ADC_SIG_NC,         /* ADC1_SE16/CMP2_IN2/ADC0_SE22 */
        ADC_SIG_PORTA | 17, /* ADC1_SE17 */
        ADC_SIG_NC,         /* VREF_OUT/CMP1_IN5/CMP0_IN5/ADC1_SE18 */
        ADC_SIG_NC,         /* 19 not implemented */
        ADC_SIG_NC,         /* 20 not implemented */
        ADC_SIG_NA,         /* 21 not implemented */
        ADC_SIG_NA,         /* 22 not implemented */
        ADC_SIG_NC          /* DAC1_OUT/CMP0_IN4/CMP2_IN3/ADC1_SE23 */
        // TODO still have 8 channels to complete, but doesn't matter for now..
    };

Modify so that it looks like this:

        case ADC_SOURCE_MODULE(2): /* ADC1 */
            if (ADC_GET_MUXSEL(source) == ADC_SOURCE_MUXSEL_A)
            {
                if(ch < 4)
                {
                    gpio_port = adc1_conv_table_a[ch];
                }
                else
                {
                    return IO_ERROR; /* channel does not exist */
                }
            }


Note: the same should be applied to other channels. But since the tower connects the potentiometer to ADC1_DM1, I only hightlight this channel.

 

You should get the reading printed on the debug screen.