How to use LPTMR KSDK driver in a FreeRTOS project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use LPTMR KSDK driver in a FreeRTOS project

How to use LPTMR KSDK driver in a FreeRTOS project

The Kinetis Software Development Kit (KSDK) is a software framework for developing applications on Kinetis MCUs. The software components in the framework include peripheral drivers, middleware and real time operating systems.

KSDK provides FreeRTOS OS, selected drivers provide FreeRTOS support in form of an additional layer. This solution enables simple driver integration in RTOS-based applications.

Drivers with FreeRTOS layers are:

• UART / LPUART / LPSCI

• I2C / LPI2C

• SPI / LPSPI

The drivers for FreeRTOS OS is a layer built on top of standard KSDK peripheral drivers to achieve multithread (RTOS) awareness. The wrappers provide an API which blocks the calling task until the I/O operation completes and allows other tasks to run in the background. This is achieved by using the asynchronous API of the underlying driver along with RTOS task synchronization objects. Underlying drivers require enabled interrupts for proper operation.

In addition, it is possible to use the KSDK bare metal drivers. This document shows how to use the LPTMR Driver in a FreeRTOS and SDK 2.0 project. For this example it is used SDK 2.0, FRDMK64F and FreeRTOS.

If you want to know how to create a new SDK 2.0 with FreeRTOS project please check the below link: https://community.freescale.com/docs/DOC-330183

GPIO AND LPTMR EXAMPLE:

Introduction

This example toggle the Blue LED every 1 second. This example check the Timer Compare Flag bit, when this flag is set blue LED changes status.

Writing the example code

  1. First it is necessary to create a new SDK 2.0 with FreeRTOS project, please check the below link for do that.

     https://community.freescale.com/docs/DOC-330183

   2. After create a new project, open the pin_mux.c file in order to enable the port clock and configure the necessary pins as GPIO (for FRDM-K64F the RGB LED is connected   through GPIO signals: RED to PTB22, BLUE to PTB21 and GREEN to PTE26).

  3. In addition, it is necessary to enable the clock for the lptmr module, in the pin_mux.c file.

  4. In main.c file it is necessary to include the fsl_lptmr.h and fsl_gpio.h.

  5. In main function, create a new task. This task will initialize the LPTMR and GPIO drivers. For this example the new task function was named task_init.

/* Create RTOS task */

   xTaskCreate(

                 task_init,

                 "Task_Init",

                 configMINIMAL_STACK_SIZE,

                 NULL,

                 task_PRIORITY,

                 NULL);

    6. Write the task_init function code.

                  a. Using the KSDK GPIO driver:

To initialize the GPIO, define a pin configuration, either input or output, in the user file. Then, call the GPIO_PinInit() function.

In this case the pin PTB21 where blue LED is connected was configured as output.

gpio_pin_config_t ledB_config = {kGPIO_DigitalOutput, 0,};

GPIO_PinInit(BOARD_LED_BLUE_GPIO, BOARD_LED_BLUE_GPIO_PIN, &ledB_config);

After configure the GPIO pins, it is possible to use the below GPIO operations:

GPIO OUTPUT OPERATIONS.

GPIO_WritePinOutput  (GPIO_Type *base, uint32_t pin, uint8_t output)

GPIO_SetPinsOutput (GPIO_Type *base, uint32_t mask)

GPIO_ClearPinsOutput (GPIO_Type *base, uint32_t mask)

GPIO_TogglePinsOutput (GPIO_Type *base, uint32_t mask)

GPIO INPUT OPERATIONS.

GPIO_ReadPinInput (GPIO_Type *base, uint32_t pin)

The board.h file contains definitions for this operations. For example:

/*!< Toggle on target LED_BLUE */

#define LED_BLUE_TOGGLE() \

GPIO_TogglePinsOutput(BOARD_LED_BLUE_GPIO, 1U << BOARD_LED_BLUE_GPIO_PIN)

                  b. Using the KSDK LPTMR driver:

The LPTMR_Init () should be called at the beginning of the application using the LPTMR driver. This function initializes the lptmr_config_t structure, this structure holds the configuration settings for the LPTMR peripheral. To initialize this structure to reasonable defaults, call the LPTMR_GetDefaultConfig () function and pass a pointer to your config structure instance. The config struct can be made const so it resides in flash.

The default values are:

config->timerMode = kLPTMR_TimerModeTimeCounter;

config->pinSelect = kLPTMR_PinSelectInput_0;

config->pinPolarity = kLPTMR_PinPolarityActiveHigh;

config->enableFreeRunning = false;

config->bypassPrescaler = true;

config->prescalerClockSource = kLPTMR_PrescalerClock_1;

config->value = kLPTMR_Prescale_Glitch_0;

After configure the LPTMR, it is necessary to set the timer period. The LPTMR_SetTimerPeriod(), the timer counts from 0 till it equals the count value set here. The count value is written to the CMR register.

Finally start the timer using the LPTMR_StarTimer (). After calling this function, the timer counts up to the CMR register value. Each time the timer reaches CMR value and then increments, it generates a trigger pulse and sets the timeout interrupt flag. An interrupt will also be triggered if the timer interrupt is enabled.

For this example the below lines configure and start the LPTMR.

/* Configure LPTMR */

LPTMR_GetDefaultConfig(&lptmrConfig);

/* Initialize the LPTMR */

LPTMR_Init(LPTMR0, &lptmrConfig);

/* Set timer period */

LPTMR_SetTimerPeriod(LPTMR0, USEC_TO_COUNT(1000000U, LPTMR_SOURCE_CLOCK));

/* Start counting */

LPTMR_StartTimer(LPTMR0);

                  c. This example check the Timer Compare Flag bit, when this flag is set blue LED changes status. So in an infinity loop the LPTMR_GetStatusFlags() function check  

                    the status flag, if this flag is set then toggle the LED and clear the flag using the the LPTMR_ClearStatusFlags() function.

while (1)

   {

   if (LPTMR_GetStatusFlags(LPTMR0) )

          {

LED_BLUE_TOGGLE();                       LPTMR_ClearStatusFlags(LPTMR0, kLPTMR_TimerCompareFlag);                }

}

  7. At this point you can build and debug the example.

Complete Code GPIO and LPTMR Example

#include <string.h>

#include "board.h"

#include "pin_mux.h"

#include "clock_config.h"

#include "fsl_debug_console.h"

#include "fsl_device_registers.h"

#include "fsl_lptmr.h"

#include "fsl_gpio.h"

/* FreeRTOS kernel includes. */

#include "FreeRTOS.h"

#include "task.h"

#include "queue.h"

#include "timers.h"

/* Task priorities. */

#define task_PRIORITY (configMAX_PRIORITIES - 1)

/*******************************************************************************

* Definitions

******************************************************************************/

/* Get source clock for LPTMR driver */

#define LPTMR_SOURCE_CLOCK CLOCK_GetFreq(kCLOCK_LpoClk)

static void task_init(void *pvParameters);

/*******************************************************************************

* Variables

******************************************************************************/

volatile uint32_t lptmrCounter = 0U;

int main(void) {

       /* Init board hardware. */

       BOARD_InitPins();

       BOARD_BootClockRUN();

       BOARD_InitDebugConsole();

       /* Add your code here */

       /* Create RTOS task */

       xTaskCreate(

                     task_init,

                     "Task_Init",

                     configMINIMAL_STACK_SIZE,

                     NULL,

                     task_PRIORITY,

                     NULL);

       vTaskStartScheduler();

       for(;;) { /* Infinite loop to avoid leaving the main function */

              __asm("NOP"); /* something to use as a breakpoint stop while looping */

       }

}

static void task_init(void *pvParameters) {

       for (;;) {

              lptmr_config_t lptmrConfig;

              PRINTF("You are running the initialization task.\r\n");

              /* Init output LED GPIO. */

              gpio_pin_config_t ledB_config = {kGPIO_DigitalOutput, 0,};

              GPIO_PinInit(BOARD_LED_BLUE_GPIO, BOARD_LED_BLUE_GPIO_PIN, &ledB_config);

              PRINTF("LED BLUE initialized \r\n");

              /* Configure LPTMR */

              /*

               * lptmrConfig.timerMode = kLPTMR_TimerModeTimeCounter;

               * lptmrConfig.pinSelect = kLPTMR_PinSelectInput_0;

               * lptmrConfig.pinPolarity = kLPTMR_PinPolarityActiveHigh;

               * lptmrConfig.enableFreeRunning = false;

               * lptmrConfig.bypassPrescaler = true;

               * lptmrConfig.prescalerClockSource = kLPTMR_PrescalerClock_1;

               * lptmrConfig.value = kLPTMR_Prescale_Glitch_0;

               */

              LPTMR_GetDefaultConfig(&lptmrConfig);

              /* Initialize the LPTMR */

              LPTMR_Init(LPTMR0, &lptmrConfig);

              /* Set timer period */

              LPTMR_SetTimerPeriod(LPTMR0, USEC_TO_COUNT(1000000U, LPTMR_SOURCE_CLOCK));

              PRINTF("Low Power Timer module initialized \r\n");

              /* Start counting */

              LPTMR_StartTimer(LPTMR0);

              while (1)

              {

                     if (LPTMR_GetStatusFlags(LPTMR0) )

                     {

                           lptmrCounter++;

                           LED_BLUE_TOGGLE();

                           LPTMR_ClearStatusFlags(LPTMR0, kLPTMR_TimerCompareFlag);

                     }

              }

       }

}

%3CLINGO-SUB%20id%3D%22lingo-sub-1100470%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E5%A6%82%E4%BD%95%E5%9C%A8FreeRTOS%E9%A1%B9%E7%9B%AE%E4%B8%AD%E4%BD%BF%E7%94%A8LPTMR%20KSDK%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1100470%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CP%3EKinetis%E8%BD%AF%E4%BB%B6%E5%BC%80%E5%8F%91%E5%A5%97%E4%BB%B6(KSDK)%E6%98%AF%E7%94%A8%E4%BA%8E%E5%9C%A8Kinetis%20MCU%E4%B8%8A%E5%BC%80%E5%8F%91%E5%BA%94%E7%94%A8%E7%9A%84%E4%B8%80%E4%B8%AA%E8%BD%AF%E4%BB%B6%E6%A1%86%E6%9E%B6%E3%80%82%20%E6%A1%86%E6%9E%B6%E4%B8%AD%E7%9A%84%E8%BD%AF%E4%BB%B6%E7%BB%84%E6%88%90%E5%8C%85%E6%8B%AC%E5%A4%96%E8%AE%BE%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E3%80%81%E4%B8%AD%E9%97%B4%E4%BB%B6%E5%92%8C%E5%AE%9E%E6%97%B6%E6%93%8D%E4%BD%9C%E7%B3%BB%E7%BB%9F%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3EKSDK%20%E6%8F%90%E4%BE%9B%20FreeRTOS%20%E6%93%8D%E4%BD%9C%E7%B3%BB%E7%BB%9F%EF%BC%8C%E9%80%89%E5%AE%9A%E7%9A%84%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E4%BB%A5%E9%99%84%E5%8A%A0%E5%B1%82%E7%9A%84%E5%BD%A2%E5%BC%8F%E6%8F%90%E4%BE%9B%20FreeRTOS%20%E6%94%AF%E6%8C%81%E3%80%82%E8%AF%A5%E8%A7%A3%E5%86%B3%E6%96%B9%E6%A1%88%E5%8F%AF%E5%9C%A8%E5%9F%BA%E4%BA%8E%20RTOS%20%E7%9A%84%E5%BA%94%E7%94%A8%E7%A8%8B%E5%BA%8F%E4%B8%AD%E5%AE%9E%E7%8E%B0%E7%AE%80%E5%8D%95%E7%9A%84%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E9%9B%86%E6%88%90%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%E5%B8%A6%E6%9C%89FreeRTOS%E5%B1%82%E7%9A%84%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E6%9C%89%EF%BC%9A%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.5in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%E2%80%A2%20UART%20%2F%20LPUART%20%2F%20LPSCI%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.5in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%E2%80%A2%20I2C%20%2F%20LPI2C%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.5in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%E2%80%A2%20SPI%20%2F%20LPSPI%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3EFreeRTOS%E6%93%8D%E4%BD%9C%E7%B3%BB%E7%BB%9F%E7%9A%84%E9%A9%B1%E5%8A%A8%E5%B1%82%E5%BB%BA%E7%AB%8B%E5%9C%A8KSDK%E6%A0%87%E5%87%86%E5%A4%96%E8%AE%BE%E9%A9%B1%E5%8A%A8%E5%B1%82%E4%B9%8B%E4%B8%8A%EF%BC%8C%E7%94%A8%E4%BB%A5%E5%AE%9E%E7%8E%B0%E5%A4%9A%E7%BA%BF%E7%A8%8B(RTOS)%E6%84%9F%E7%9F%A5%E3%80%82%20%E5%8C%85%E8%A3%85%E5%99%A8%E6%8F%90%E4%BE%9B%E7%9A%84API%E5%8F%AF%E9%98%BB%E5%A1%9E%E8%B0%83%E7%94%A8%E4%BB%BB%E5%8A%A1%EF%BC%8C%E7%9B%B4%E5%88%B0I%2FO%E6%93%8D%E4%BD%9C%E5%AE%8C%E6%88%90%EF%BC%8C%E5%85%81%E8%AE%B8%E5%85%B6%E4%BB%96%E4%BB%BB%E5%8A%A1%E5%9C%A8%E5%90%8E%E5%8F%B0%E8%BF%90%E8%A1%8C%E3%80%82%20%E8%AF%A5%E7%89%B9%E6%80%A7%E7%9A%84%E5%AE%9E%E7%8E%B0%E9%9C%80%E8%A6%81%E4%BD%BF%E7%94%A8%E5%BA%95%E5%B1%82%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E7%9A%84%E5%BC%82%E6%AD%A5API%E4%BB%A5%E5%8F%8ARTOS%E4%BB%BB%E5%8A%A1%E5%90%8C%E6%AD%A5%E5%AF%B9%E8%B1%A1%E3%80%82%20%E5%BA%95%E5%B1%82%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E9%9C%80%E8%A6%81%E5%90%AF%E7%94%A8%E4%B8%AD%E6%96%AD%E4%BB%A5%E7%A1%AE%E4%BF%9D%E6%AD%A3%E5%B8%B8%E6%93%8D%E4%BD%9C%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%E6%AD%A4%E5%A4%96%3CSTRONG%3E%EF%BC%8C%E8%BF%98%E5%8F%AF%E4%BB%A5%E4%BD%BF%E7%94%A8%20KSDK%20%E8%A3%B8%E6%9C%BA%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%3C%2FSTRONG%3E%E3%80%82%E6%9C%AC%E6%96%87%E6%A1%A3%E4%BB%8B%E7%BB%8D%E5%A6%82%E4%BD%95%E5%9C%A8%20FreeRTOS%20%E5%92%8C%20SDK%202.0%20%E9%A1%B9%E7%9B%AE%E4%B8%AD%E4%BD%BF%E7%94%A8%20LPTMR%20%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E3%80%82%E6%9C%AC%E4%BE%8B%E4%B8%AD%E4%BD%BF%E7%94%A8%E4%BA%86%20SDK%202.0%E3%80%81FRDMK64F%20%E5%92%8C%20FreeRTOS%E3%80%82%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%3CSPAN%3E%E5%A6%82%E6%9E%9C%E6%82%A8%E6%83%B3%E4%BA%86%E8%A7%A3%E5%A6%82%E4%BD%95%E4%BD%BF%E7%94%A8%20FreeRTOS%20%E9%A1%B9%E7%9B%AE%E5%88%9B%E5%BB%BA%E6%96%B0%E7%9A%84%20SDK%202.0%EF%BC%8C%E8%AF%B7%E6%9F%A5%E7%9C%8B%E4%BB%A5%E4%B8%8B%E9%93%BE%E6%8E%A5%EF%BC%9A%3C%2FSPAN%3E%20%3CA%20class%3D%22jive-link-external-small%22%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Fexternal-link.jspa%3Furl%3Dhttps%253A%252F%252Fcommunity.freescale.com%252Fdocs%252FDOC-330183%22%20target%3D%22_blank%22%3Ehttps%3A%2F%2Fcommunity.freescale.com%2Fdocs%2FDOC-330183%3C%2FA%3E%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%20style%3D%22text-align%3A%20justify%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2014.0pt%3B%22%3E%3CSTRONG%3EGPIO%20%E5%92%8C%20LPTMR%20%E7%A4%BA%E4%BE%8B%EF%BC%9A%3C%2FSTRONG%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22text-align%3A%20justify%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2014.0pt%3B%22%3E%3CSTRONG%3E%E7%AE%80%E4%BB%8B%3C%2FSTRONG%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%E6%AD%A4%E7%A4%BA%E4%BE%8B%E6%AF%8F%201%20%E7%A7%92%E5%88%87%E6%8D%A2%E4%B8%80%E6%AC%A1%E8%93%9D%E8%89%B2%20LED%E3%80%82%E6%AD%A4%E7%A4%BA%E4%BE%8B%E6%A3%80%E6%9F%A5%E5%AE%9A%E6%97%B6%E5%99%A8%E6%AF%94%E8%BE%83%E6%A0%87%E5%BF%97%E4%BD%8D%EF%BC%8C%E5%BD%93%E8%AE%BE%E7%BD%AE%E6%AD%A4%E6%A0%87%E5%BF%97%E6%97%B6%EF%BC%8C%E8%93%9D%E8%89%B2%20LED%20%E4%BC%9A%E6%94%B9%E5%8F%98%E7%8A%B6%E6%80%81%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22text-align%3A%20justify%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2014.0pt%3B%22%3E%3CSTRONG%3E%E7%BC%96%E5%86%99%E7%A4%BA%E4%BE%8B%E4%BB%A3%E7%A0%81%3C%2FSTRONG%3E%3C%2FSPAN%3E%3C%2FP%3E%3COL%3E%3CLI%3E%E9%A6%96%E5%85%88%E9%9C%80%E8%A6%81%E5%88%9B%E5%BB%BA%E4%B8%80%E4%B8%AA%E5%B8%A6%E6%9C%89%20FreeRTOS%20%E9%A1%B9%E7%9B%AE%E7%9A%84%E6%96%B0%20SDK%202.0%EF%BC%8C%E8%AF%B7%E6%9F%A5%E7%9C%8B%E4%BB%A5%E4%B8%8B%E9%93%BE%E6%8E%A5%E8%BF%9B%E8%A1%8C%E6%93%8D%E4%BD%9C%E3%80%82%3C%2FLI%3E%3C%2FOL%3E%3CP%20style%3D%22text-align%3A%20justify%3B%22%3E%3CSPAN%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%3C%2FSPAN%3E%3CA%20class%3D%22jive-link-external-small%22%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Fexternal-link.jspa%3Furl%3Dhttps%253A%252F%252Fcommunity.freescale.com%252Fdocs%252FDOC-330183%22%20target%3D%22_blank%22%3Ehttps%3A%2F%2Fcommunity.freescale.com%2Fdocs%2FDOC-330183%3C%2FA%3E%3C%2FP%3E%3CP%20style%3D%22text-align%3A%20justify%3B%22%3E%3C%2FP%3E%3CP%3E2.%E5%88%9B%E5%BB%BA%E6%96%B0%E9%A1%B9%E7%9B%AE%E5%90%8E%EF%BC%8C%E6%89%93%E5%BC%80pin_mux.c%E6%96%87%E4%BB%B6%E4%BB%A5%E5%90%AF%E7%94%A8%E7%AB%AF%E5%8F%A3%E6%97%B6%E9%92%9F%E5%B9%B6%E5%B0%86%E5%BF%85%E8%A6%81%E7%9A%84%E5%BC%95%E8%84%9A%E9%85%8D%E7%BD%AE%E4%B8%BA%20GPIO%EF%BC%88%E5%AF%B9%E4%BA%8E%20FRDM-K64F%EF%BC%8CRGB%20LED%20%E9%80%9A%E8%BF%87%20GPIO%20%E4%BF%A1%E5%8F%B7%E8%BF%9E%E6%8E%A5%EF%BC%9A%E7%BA%A2%E8%89%B2%E5%88%B0%20PTB22%EF%BC%8C%E8%93%9D%E8%89%B2%E5%88%B0%20PTB21%20%E4%BB%A5%E5%8F%8A%E7%BB%BF%E8%89%B2%E5%88%B0%20PTE26%EF%BC%89%E3%80%82%3C%2FP%3E%3CP%20style%3D%22text-align%3A%20justify%3B%22%3E%3C%2FP%3E%3CP%3E3.%E6%AD%A4%E5%A4%96%EF%BC%8C%E8%BF%98%E9%9C%80%E8%A6%81%E5%9C%A8%20pin_mux.c%20%E4%B8%AD%E5%90%AF%E7%94%A8%20lptmr%20%E6%A8%A1%E5%9D%97%E7%9A%84%E6%97%B6%E9%92%9F%E6%96%87%E4%BB%B6%E3%80%82%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%20style%3D%22text-align%3A%20justify%3B%22%3E4.%E5%9C%A8%20main.c%20%E4%B8%AD%E6%96%87%E4%BB%B6%E9%9C%80%E8%A6%81%E5%8C%85%E5%90%AB%20fsl_lptmr.h%E5%92%8Cfsl_gpio.h%E3%80%82%3C%2FP%3E%3CP%20style%3D%22text-align%3A%20justify%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22text-align%3A%20justify%3B%22%3E5.%E5%9C%A8%E4%B8%BB%E5%87%BD%E6%95%B0%E4%B8%AD%EF%BC%8C%E5%88%9B%E5%BB%BA%E4%B8%80%E4%B8%AA%E6%96%B0%E4%BB%BB%E5%8A%A1%E3%80%82%E6%AD%A4%E4%BB%BB%E5%8A%A1%E5%B0%86%E5%88%9D%E5%A7%8B%E5%8C%96%20LPTMR%20%E5%92%8C%20GPIO%20%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E3%80%82%E5%AF%B9%E4%BA%8E%E6%AD%A4%E7%A4%BA%E4%BE%8B%EF%BC%8C%E6%96%B0%E7%9A%84%E4%BB%BB%E5%8A%A1%E5%87%BD%E6%95%B0%E8%A2%AB%E5%91%BD%E5%90%8D%E4%B8%BA%20task_init%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.25in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%20%E5%88%9B%E5%BB%BA%20RTOS%20%E4%BB%BB%E5%8A%A1%20*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.25in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ExTaskCreate%EF%BC%88%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.25in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E4%BB%BB%E5%8A%A1%E5%88%9D%E5%A7%8B%E5%8C%96%EF%BC%8C%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.25in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%E2%80%9C%E4%BB%BB%E5%8A%A1%E5%88%9D%E5%A7%8B%E5%8C%96%E2%80%9D%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%EF%BC%8C%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.25in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E9%85%8D%E7%BD%AE%E6%9C%80%E5%B0%8F%E5%A0%86%E6%A0%88%E5%A4%A7%E5%B0%8F%EF%BC%8C%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.25in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E6%97%A0%E6%95%88%E7%9A%84%EF%BC%8C%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.25in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E4%BB%BB%E5%8A%A1%E4%BC%98%E5%85%88%E7%BA%A7%EF%BC%8C%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.25in%3B%20text-align%3A%20justify%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20NULL)%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%3C%2FP%3E%3CP%3E6.%E7%BC%96%E5%86%99task_init%E5%87%BD%E6%95%B0%E4%BB%A3%E7%A0%81%E3%80%82%3C%2FP%3E%3CP%3E%3CSTRONG%3Ea.%E4%BD%BF%E7%94%A8KSDK%20GPIO%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%EF%BC%9A%20%3C%2FSTRONG%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%E8%A6%81%E5%88%9D%E5%A7%8B%E5%8C%96%20GPIO%EF%BC%8C%E8%AF%B7%E5%9C%A8%E7%94%A8%E6%88%B7%E6%96%87%E4%BB%B6%E4%B8%AD%E5%AE%9A%E4%B9%89%E5%BC%95%E8%84%9A%E9%85%8D%E7%BD%AE%EF%BC%88%E8%BE%93%E5%85%A5%E6%88%96%E8%BE%93%E5%87%BA%EF%BC%89%E3%80%82%E7%84%B6%E5%90%8E%EF%BC%8C%E8%B0%83%E7%94%A8%3CSPAN%20style%3D%22color%3A%20windowtext%3B%22%3EGPIO_PinInit()%3C%2FSPAN%3E%3CSPAN%20style%3D%22text-align%3A%20start%3B%22%3E%E5%87%BD%E6%95%B0%E3%80%82%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%E5%9C%A8%E8%BF%99%E7%A7%8D%E6%83%85%E5%86%B5%E4%B8%8B%EF%BC%8C%E8%BF%9E%E6%8E%A5%E8%93%9D%E8%89%B2%20LED%20%E7%9A%84%E5%BC%95%E8%84%9A%20PTB21%20%E8%A2%AB%E9%85%8D%E7%BD%AE%E4%B8%BA%E8%BE%93%E5%87%BA%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.25in%3B%20margin-bottom%3A%200.0001pt%3B%20text-indent%3A%200.5in%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%23005032%3B%22%3Egpio_pin_config_t%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20ledB_config%20%3D%20%7B%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%230000c0%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CEM%3EkGPIO_DigitalOutput%3C%2FEM%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%2C%200%2C%7D%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EGPIO_PinInit(BOARD_LED_BLUE_GPIO%2C%20BOARD_LED_BLUE_GPIO_PIN%2C%20%26amp%3BledB_config)%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%E9%85%8D%E7%BD%AEGPIO%E5%BC%95%E8%84%9A%E5%90%8E%EF%BC%8C%E5%8F%AF%E4%BB%A5%E4%BD%BF%E7%94%A8%E4%BB%A5%E4%B8%8BGPIO%E6%93%8D%E4%BD%9C%EF%BC%9A%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3EGPIO%20%E8%BE%93%E5%87%BA%E6%93%8D%E4%BD%9C%E3%80%82%3C%2FP%3E%3CP%20style%3D%22padding-left%3A%2090px%3B%22%3E%3CEM%3EGPIO_WritePinOutput%26nbsp%3B%20(GPIO_Type%20*base%2C%20uint32_t%20pin%2C%20uint8_t%20output)%3C%2FEM%3E%3C%2FP%3E%3CP%20style%3D%22padding-left%3A%2090px%3B%22%3E%3CEM%3EGPIO_SetPinsOutput%EF%BC%88GPIO_Type%20*base%EF%BC%8Cuint32_t%20mask%EF%BC%89%3C%2FEM%3E%3C%2FP%3E%3CP%20style%3D%22padding-left%3A%2090px%3B%22%3E%3CEM%3EGPIO_ClearPinsOutput%EF%BC%88GPIO_Type%20*base%EF%BC%8Cuint32_t%20mask%EF%BC%89%3C%2FEM%3E%3C%2FP%3E%3CP%20style%3D%22padding-left%3A%2090px%3B%22%3E%3CEM%3EGPIO_TogglePinsOutput%EF%BC%88GPIO_Type%20*base%EF%BC%8Cuint32_t%20mask%EF%BC%89%3C%2FEM%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3EGPIO%20%E8%BE%93%E5%85%A5%E6%93%8D%E4%BD%9C%E3%80%82%3C%2FP%3E%3CP%20style%3D%22padding-left%3A%2090px%3B%22%3E%3CEM%3EGPIO_ReadPinInput%20%3CSPAN%20style%3D%22text-align%3A%20start%3B%22%3E%EF%BC%88GPIO_Type%20*base%EF%BC%8Cuint32_t%20pin%EF%BC%89%3C%2FSPAN%3E%3C%2FEM%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3Eboard.h%20%E6%96%87%E4%BB%B6%E5%8C%85%E5%90%AB%E6%AD%A4%E6%93%8D%E4%BD%9C%E7%9A%84%E5%AE%9A%E4%B9%89%E3%80%82%E4%BE%8B%E5%A6%82%EF%BC%9A%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*!%26lt%3B%20%E5%88%87%E6%8D%A2%E7%9B%AE%E6%A0%87%20LED_BLUE%20*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.25in%3B%20margin-bottom%3A%200.0001pt%3B%20text-indent%3A%200.5in%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%23%E5%AE%9A%E4%B9%89%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ELED_BLUE_TOGGLE%EF%BC%88%EF%BC%89%5C%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.25in%3B%20margin-bottom%3A%200.0001pt%3B%20text-indent%3A%200.5in%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EGPIO_TogglePinsOutput%EF%BC%88%E6%9D%BF_LED_BLUE_GPIO%EF%BC%8C1U%20%26lt%3B%26lt%3B%20%E6%9D%BF_LED_BLUE_GPIO_PIN%EF%BC%89%20%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%3C%2FP%3E%3CP%3E%3CSTRONG%3Eb.%E4%BD%BF%E7%94%A8%20KSDK%20LPTMR%20%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%EF%BC%9A%3C%2FSTRONG%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20start%3B%20background%3A%20white%20none%20repeat%20scroll%200%25%200%25%3B%22%3E%E5%BA%94%E5%9C%A8%E5%BA%94%E7%94%A8%E7%A8%8B%E5%BA%8F%E5%BC%80%E5%A7%8B%E6%97%B6%E4%BD%BF%E7%94%A8%20LPTMR%20%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E8%B0%83%E7%94%A8%20LPTMR_Init%20()%E3%80%82%E6%AD%A4%E5%87%BD%E6%95%B0%E5%88%9D%E5%A7%8B%E5%8C%96%20lptmr_config_t%20%E7%BB%93%E6%9E%84%EF%BC%8C%E8%AF%A5%E7%BB%93%E6%9E%84%E4%BF%9D%E5%AD%98%20LPTMR%20%E5%A4%96%E8%AE%BE%E7%9A%84%E9%85%8D%E7%BD%AE%E8%AE%BE%E7%BD%AE%E3%80%82%E8%A6%81%E5%B0%86%E6%AD%A4%E7%BB%93%E6%9E%84%E5%88%9D%E5%A7%8B%E5%8C%96%E4%B8%BA%E5%90%88%E7%90%86%E7%9A%84%E9%BB%98%E8%AE%A4%E5%80%BC%EF%BC%8C%E8%AF%B7%E8%B0%83%E7%94%A8%20LPTMR_GetDefaultConfig%20()%20%E5%87%BD%E6%95%B0%E5%B9%B6%E5%B0%86%E6%8C%87%E9%92%88%E4%BC%A0%E9%80%92%E7%BB%99%E6%82%A8%E7%9A%84%E9%85%8D%E7%BD%AE%E7%BB%93%E6%9E%84%E5%AE%9E%E4%BE%8B%E3%80%82%E9%85%8D%E7%BD%AE%E7%BB%93%E6%9E%84%E5%8F%AF%E4%BB%A5%E8%AE%BE%E4%B8%BA%20const%EF%BC%8C%E4%BB%A5%E4%BE%BF%E5%AE%83%E9%A9%BB%E7%95%99%E5%9C%A8%E9%97%AA%E5%AD%98%E4%B8%AD%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%20background%3A%20white%20none%20repeat%20scroll%200%25%200%25%3B%22%3E%E9%BB%98%E8%AE%A4%E5%80%BC%E4%B8%BA%EF%BC%9A%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%2093.75pt%3B%20margin-bottom%3A%200.0001pt%3B%20text-indent%3A%20-39.75pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%2093.75pt%3B%20margin-bottom%3A%200.0001pt%3B%20text-indent%3A%20-39.75pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20'Courier%20New'%3B%20color%3A%20%2351626f%3B%22%3E%E9%85%8D%E7%BD%AE-%26gt%3BtimerMode%20%3D%20kLPTMR_TimerModeTimeCounter%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%2093.75pt%3B%20margin-bottom%3A%200.0001pt%3B%20text-indent%3A%20-39.75pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20'Courier%20New'%3B%20color%3A%20%2351626f%3B%22%3E%E9%85%8D%E7%BD%AE-%26gt%3BpinSelect%20%3D%20kLPTMR_PinSelectInput_0%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%2093.75pt%3B%20margin-bottom%3A%200.0001pt%3B%20text-indent%3A%20-39.75pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20'Courier%20New'%3B%20color%3A%20%2351626f%3B%22%3E%E9%85%8D%E7%BD%AE-%26gt%3BpinPolarity%20%3D%20kLPTMR_PinPolarityActiveHigh%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%2093.75pt%3B%20margin-bottom%3A%200.0001pt%3B%20text-indent%3A%20-39.75pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20'Courier%20New'%3B%20color%3A%20%2351626f%3B%22%3E%E9%85%8D%E7%BD%AE-%26gt%3B%E5%90%AF%E7%94%A8%E8%87%AA%E7%94%B1%E8%BF%90%E8%A1%8C%20%3D%20false%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%2093.75pt%3B%20margin-bottom%3A%200.0001pt%3B%20text-indent%3A%20-39.75pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20'Courier%20New'%3B%20color%3A%20%2351626f%3B%22%3Econfig-%26gt%3BbypassPrescaler%20%3D%20true%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%2093.75pt%3B%20margin-bottom%3A%200.0001pt%3B%20text-indent%3A%20-39.75pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20'Courier%20New'%3B%20color%3A%20%2351626f%3B%22%3E%E9%85%8D%E7%BD%AE-%26gt%3B%E9%A2%84%E5%88%86%E9%A2%91%E5%99%A8%E6%97%B6%E9%92%9F%E6%BA%90%3DkLPTMR_PrescalerClock_1%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%2093.75pt%3B%20margin-bottom%3A%200.0001pt%3B%20text-indent%3A%20-39.75pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20'Courier%20New'%3B%20color%3A%20%2351626f%3B%22%3Econfig-%26gt%3Bvalue%20%3D%20kLPTMR_Prescale_Glitch_0%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%2093.75pt%3B%20margin-bottom%3A%200.0001pt%3B%20text-indent%3A%20-39.75pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%20background%3A%20white%20none%20repeat%20scroll%200%25%200%25%3B%22%3E%E9%85%8D%E7%BD%AELPTMR%E5%90%8E%EF%BC%8C%E9%9C%80%E8%A6%81%E8%AE%BE%E7%BD%AE%E5%AE%9A%E6%97%B6%E5%99%A8%E5%91%A8%E6%9C%9F%E3%80%82LPTMR_SetTimerPeriod()%EF%BC%8C%E8%AE%A1%E6%97%B6%E5%99%A8%E4%BB%8E0%E5%BC%80%E5%A7%8B%E8%AE%A1%E6%95%B0%EF%BC%8C%E7%9B%B4%E5%88%B0%E7%AD%89%E4%BA%8E%E6%AD%A4%E5%A4%84%E8%AE%BE%E7%BD%AE%E7%9A%84%E8%AE%A1%E6%95%B0%E5%80%BC%E3%80%82%E8%AE%A1%E6%95%B0%E5%80%BC%E5%86%99%E5%85%A5CMR%E5%AF%84%E5%AD%98%E5%99%A8%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%20background%3A%20white%20none%20repeat%20scroll%200%25%200%25%3B%22%3E%E6%9C%80%E5%90%8E%E4%BD%BF%E7%94%A8LPTMR_StarTimer()%E5%90%AF%E5%8A%A8%E8%AE%A1%E6%97%B6%E5%99%A8%E3%80%82%E8%B0%83%E7%94%A8%E6%AD%A4%E5%87%BD%E6%95%B0%E5%90%8E%EF%BC%8C%E5%AE%9A%E6%97%B6%E5%99%A8%E8%AE%A1%E6%95%B0%E8%87%B3CMR%E5%AF%84%E5%AD%98%E5%99%A8%E7%9A%84%E5%80%BC%E3%80%82%E6%AF%8F%E6%AC%A1%E5%AE%9A%E6%97%B6%E5%99%A8%E8%BE%BE%E5%88%B0CMR%E5%80%BC%E7%84%B6%E5%90%8E%E9%80%92%E5%A2%9E%E6%97%B6%EF%BC%8C%E5%AE%83%E9%83%BD%E4%BC%9A%E4%BA%A7%E7%94%9F%E4%B8%80%E4%B8%AA%E8%A7%A6%E5%8F%91%E8%84%89%E5%86%B2%E5%B9%B6%E8%AE%BE%E7%BD%AE%E8%B6%85%E6%97%B6%E4%B8%AD%E6%96%AD%E6%A0%87%E5%BF%97%E3%80%82%E5%A6%82%E6%9E%9C%E5%90%AF%E7%94%A8%E5%AE%9A%E6%97%B6%E5%99%A8%E4%B8%AD%E6%96%AD%EF%BC%8C%E4%B9%9F%E4%BC%9A%E8%A7%A6%E5%8F%91%E4%B8%AD%E6%96%AD%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%20background%3A%20white%20none%20repeat%20scroll%200%25%200%25%3B%22%3E%E5%AF%B9%E4%BA%8E%E6%AD%A4%E7%A4%BA%E4%BE%8B%EF%BC%8C%E4%BB%A5%E4%B8%8B%E5%87%A0%E8%A1%8C%E9%85%8D%E7%BD%AE%E5%B9%B6%E5%90%AF%E5%8A%A8%20LPTMR%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%20%E9%85%8D%E7%BD%AE%20LPTMR%20*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ELPTMR_GetDefaultConfig(%26amp%3BlptmrConfig)%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%E5%88%9D%E5%A7%8B%E5%8C%96LPTMR*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ELPTMR_Init(LPTMR0%2C%20%26amp%3BlptmrConfig)%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%20%E8%AE%BE%E7%BD%AE%E5%AE%9A%E6%97%B6%E5%99%A8%E5%91%A8%E6%9C%9F%20*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ELPTMR_SetTimerPeriod%EF%BC%88LPTMR0%EF%BC%8CUSEC_TO_COUNT%EF%BC%881000000U%EF%BC%8CLPTMR_SOURCE_CLOCK%EF%BC%89%EF%BC%89%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%20%E5%BC%80%E5%A7%8B%E8%AE%A1%E6%95%B0%20*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ELPTMR_StartTimer(LPTMR0)%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%3E%3CSTRONG%3E%3CSPAN%20style%3D%22color%3A%20%23606060%3B%22%3Ec.%3C%2FSPAN%3E%3C%2FSTRONG%3E%E6%AD%A4%E7%A4%BA%E4%BE%8B%E6%A3%80%E6%9F%A5%E5%AE%9A%E6%97%B6%E5%99%A8%E6%AF%94%E8%BE%83%E6%A0%87%E5%BF%97%E4%BD%8D%EF%BC%8C%E5%BD%93%E8%AE%BE%E7%BD%AE%E6%AD%A4%E6%A0%87%E5%BF%97%E6%97%B6%EF%BC%8C%E8%93%9D%E8%89%B2%20LED%20%E4%BC%9A%E6%94%B9%E5%8F%98%E7%8A%B6%E6%80%81%E3%80%82%E5%9B%A0%E6%AD%A4%EF%BC%8C%E5%9C%A8%E6%97%A0%E9%99%90%E5%BE%AA%E7%8E%AF%E4%B8%AD%EF%BC%8CLPTMR_GetStatusFlags()%20%E5%87%BD%E6%95%B0%E6%A3%80%E6%9F%A5%3C%2FP%3E%3CP%3E%E7%8A%B6%E6%80%81%E6%A0%87%E5%BF%97%EF%BC%8C%E5%A6%82%E6%9E%9C%E8%AE%BE%E7%BD%AE%E4%BA%86%E6%AD%A4%E6%A0%87%E5%BF%97%EF%BC%8C%E5%88%99%E5%88%87%E6%8D%A2%20LED%20%E5%B9%B6%E4%BD%BF%E7%94%A8%20LPTMR_ClearStatusFlags()%20%E5%87%BD%E6%95%B0%E6%B8%85%E9%99%A4%E6%A0%87%E5%BF%97%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Ewhile%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%EF%BC%881%EF%BC%89%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%26nbsp%3B%20%7B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%20%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Eif%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20(LPTMR_GetStatusFlags(LPTMR0)%20)%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%7B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%201in%3B%20margin-bottom%3A%200.0001pt%3B%20text-indent%3A%200.5in%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ELED_BLUE_TOGGLE()%3B%20LPTMR_ClearStatusFlags(LPTMR0%EF%BC%8C%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%230000c0%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CEM%3EkLPTMR_TimerCompareFlag%3C%2FEM%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%3B%20%7D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%200.75in%3B%20margin-bottom%3A%200.0001pt%3B%20text-align%3A%20justify%3B%20text-indent%3A%200.25in%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%3E7.%E6%AD%A4%E6%97%B6%E6%82%A8%E5%8F%AF%E4%BB%A5%E6%9E%84%E5%BB%BA%E5%B9%B6%E8%B0%83%E8%AF%95%E7%A4%BA%E4%BE%8B%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2014.0pt%3B%22%3E%3CSTRONG%3E%E5%AE%8C%E6%95%B4%E4%BB%A3%E7%A0%81GPIO%E5%92%8CLPTMR%E7%A4%BA%E4%BE%8B%3C%2FSTRONG%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%23include%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%3CSTRING.H%3E%3C%2FSTRING.H%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%23%E5%8C%85%E6%8B%AC%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%E2%80%9Cboard.h%E2%80%9D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%23%E5%8C%85%E6%8B%AC%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%E2%80%9Cpin_mux.h%E2%80%9D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%23%E5%8C%85%E6%8B%AC%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%E2%80%9Cclock_config.h%E2%80%9D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%23%E5%8C%85%E6%8B%AC%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%E2%80%9Cfsl_debug_console.h%E2%80%9D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%23%E5%8C%85%E6%8B%AC%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%E2%80%9Cfsl_device_registers.h%E2%80%9D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%23%E5%8C%85%E6%8B%AC%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%E2%80%9Cfsl_lptmr.h%E2%80%9D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%23%E5%8C%85%E6%8B%AC%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%E2%80%9Cfsl_gpio.h%E2%80%9D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%20FreeRTOS%20%E5%86%85%E6%A0%B8%E5%8C%85%E6%8B%AC%E3%80%82*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%23%E5%8C%85%E6%8B%AC%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%E2%80%9CFreeRTOS.h%E2%80%9D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%23%E5%8C%85%E6%8B%AC%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%E2%80%9C%E4%BB%BB%E5%8A%A1.h%E2%80%9D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%23include%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%22%E9%98%9F%E5%88%97.h%22%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%23%E5%8C%85%E6%8B%AC%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%E2%80%9C%E8%AE%A1%E6%97%B6%E5%99%A8.h%E2%80%9D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%20%E4%BB%BB%E5%8A%A1%E4%BC%98%E5%85%88%E7%BA%A7%E3%80%82*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%23%E5%AE%9A%E4%B9%89%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E4%BB%BB%E5%8A%A1%E4%BC%98%E5%85%88%E7%BA%A7%EF%BC%88configMAX_PRIORITIES-1%EF%BC%89%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*******************************************************************************%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20*%20%E5%AE%9A%E4%B9%89%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20******************************************************************************%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%20%E8%8E%B7%E5%8F%96%20LPTMR%20%E9%A9%B1%E5%8A%A8%E7%A8%8B%E5%BA%8F%E7%9A%84%E6%BA%90%E6%97%B6%E9%92%9F%20*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%23%E5%AE%9A%E4%B9%89%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ELPTMR_SOURCE_CLOCK%20CLOCK_GetFreq%EF%BC%88kCLOCK_LpoClk%EF%BC%89%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Estatic%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20%3CSTRONG%3Etask_init%3C%2FSTRONG%3E(%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20*pvParameters)%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*******************************************************************************%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20*%20Variables%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%20******************************************************************************%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Evolatile%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%23005032%3B%22%3Euint32_t%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20lptmrCounter%20%3D%200U%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Eint%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%3CSTRONG%3Emain%3C%2FSTRONG%3E%20%EF%BC%88%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%EF%BC%89%7B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%3CSPAN%20style%3D%22text-decoration%3A%20underline%3B%22%3E%E5%88%9D%E5%A7%8B%E5%8C%96%3C%2FSPAN%3E%E6%9D%BF%E7%A1%AC%E4%BB%B6%E3%80%82%20*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E6%9D%BF%E5%88%9D%E5%A7%8B%E5%8C%96%E5%BC%95%E8%84%9A%EF%BC%88%EF%BC%89%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E4%B8%BB%E6%9D%BF%E5%90%AF%E5%8A%A8%E6%97%B6%E9%92%9F%E8%BF%90%E8%A1%8C%EF%BC%88%EF%BC%89%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20BOARD_InitDebugConsole()%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%20%E5%9C%A8%E8%BF%99%E9%87%8C%E6%B7%BB%E5%8A%A0%E6%82%A8%E7%9A%84%E4%BB%A3%E7%A0%81%20*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%20%E5%88%9B%E5%BB%BA%20RTOS%20%E4%BB%BB%E5%8A%A1%20*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ExTaskCreate%EF%BC%88%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E4%BB%BB%E5%8A%A1%E5%88%9D%E5%A7%8B%E5%8C%96%EF%BC%8C%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%E2%80%9C%E4%BB%BB%E5%8A%A1%E5%88%9D%E5%A7%8B%E5%8C%96%E2%80%9D%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%EF%BC%8C%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E9%85%8D%E7%BD%AE%E6%9C%80%E5%B0%8F%E5%A0%86%E6%A0%88%E5%A4%A7%E5%B0%8F%EF%BC%8C%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E6%97%A0%E6%95%88%E7%9A%84%EF%BC%8C%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%E4%BB%BB%E5%8A%A1%E4%BC%98%E5%85%88%E7%BA%A7%EF%BC%8C%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20NULL)%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EvTaskStartScheduler()%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Efor%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E(%3B%3B)%20%7B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%20%E6%97%A0%E9%99%90%E5%BE%AA%E7%8E%AF%E4%BB%A5%E9%81%BF%E5%85%8D%E7%A6%BB%E5%BC%80%E4%B8%BB%E5%87%BD%E6%95%B0%20*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E__asm%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E(%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%22NOP%22%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20%3B%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%20%E5%BE%AA%E7%8E%AF%E6%97%B6%E7%94%A8%E4%BD%9C%E6%96%AD%E7%82%B9%E5%81%9C%E6%AD%A2%E7%9A%84%E4%B8%9C%E8%A5%BF%20*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%7D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Estatic%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20%3CSTRONG%3Etask_init%3C%2FSTRONG%3E(%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Evoid%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20*pvParameters)%20%7B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3E%E4%B8%BA%E4%BA%86%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%EF%BC%88%3B%3B%EF%BC%89%20%7B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%23005032%3B%22%3Elptmr_config_t%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20lptmrConfig%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EPRINTF(%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%22%E6%82%A8%E6%AD%A3%E5%9C%A8%E8%BF%90%E8%A1%8C%E5%88%9D%E5%A7%8B%E5%8C%96%E4%BB%BB%E5%8A%A1%E3%80%82%5Cr%5Cn%22%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%3CSPAN%20style%3D%22text-decoration%3A%20underline%3B%22%3E%E5%88%9D%E5%A7%8B%E5%8C%96%3C%2FSPAN%3E%E8%BE%93%E5%87%BA%20LED%20GPIO%E3%80%82*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%23005032%3B%22%3Egpio_pin_config_t%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20ledB_config%20%3D%20%7B%3C%2FSPAN%3E%3CSPAN%20style%3D%22color%3A%20%230000c0%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CEM%3EkGPIO_DigitalOutput%3C%2FEM%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%2C%200%2C%7D%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20GPIO_PinInit(BOARD_LED_BLUE_GPIO%2C%20BOARD_LED_BLUE_GPIO_PIN%2C%20%26amp%3BledB_config)%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EPRINTF(%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%22LED%20%E8%93%9D%E8%89%B2%E5%88%9D%E5%A7%8B%E5%8C%96%20%5Cr%5Cn%22%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%20%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%20%E9%85%8D%E7%BD%AE%20LPTMR%20*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20*%20lptmrConfig.timerMode%20%3D%20kLPTMR_TimerModeTimeCounter%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20*%20lptmrConfig.pinSelect%20%3D%20kLPTMR_PinSelectInput_0%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E*lptmrConfig.pinPolarity%20%3D%20kLPTMR_PinPolarityActiveHigh%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E*%20lptmrConfig.enableFreeRunning%3D%E5%81%87%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20*%20lptmrConfig.bypassPrescaler%20%3D%20true%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E*%20lptmrConfig.%E9%A2%84%E5%88%86%E9%A2%91%E5%99%A8%E6%97%B6%E9%92%9F%E6%BA%90%3DkLPTMR_%E9%A2%84%E5%88%86%E9%A2%91%E5%99%A8%E6%97%B6%E9%92%9F_1%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20*%20lptmrConfig.value%20%3D%20kLPTMR_Prescale_Glitch_0%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20LPTMR_GetDefaultConfig(%26amp%3BlptmrConfig)%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%E5%88%9D%E5%A7%8B%E5%8C%96LPTMR*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20LPTMR_Init(LPTMR0%2C%20%26amp%3BlptmrConfig)%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%20%E8%AE%BE%E7%BD%AE%E5%AE%9A%E6%97%B6%E5%99%A8%E5%91%A8%E6%9C%9F%20*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ELPTMR_SetTimerPeriod%EF%BC%88LPTMR0%EF%BC%8CUSEC_TO_COUNT%EF%BC%881000000U%EF%BC%8CLPTMR_SOURCE_CLOCK%EF%BC%89%EF%BC%89%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3EPRINTF(%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%232a00ff%3B%22%3E%22%E4%BD%8E%E5%8A%9F%E8%80%97%E5%AE%9A%E6%97%B6%E5%99%A8%E6%A8%A1%E5%9D%97%E5%B7%B2%E5%88%9D%E5%A7%8B%E5%8C%96%20%5Cr%5Cn%22%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E)%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20%233f7f5f%3B%22%3E%2F*%20%E5%BC%80%E5%A7%8B%E8%AE%A1%E6%95%B0%20*%2F%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20LPTMR_StartTimer(LPTMR0)%3B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Ewhile%3C%2FSTRONG%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%EF%BC%881%EF%BC%89%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%3CSPAN%20style%3D%22color%3A%20%237f0055%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CSTRONG%3Eif%3C%2FSTRONG%3E%3C%2FSPAN%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%20(LPTMR_GetStatusFlags(LPTMR0)%20)%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3Elptmr%E8%AE%A1%E6%95%B0%E5%99%A8%2B%2B%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ELED_%E8%93%9D%E8%89%B2_%E5%88%87%E6%8D%A2%EF%BC%88%EF%BC%89%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3ELPTMR_ClearStatusFlags%EF%BC%88LPTMR0%EF%BC%8C%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22color%3A%20%230000c0%3B%20font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%22%3E%3CEM%3EkLPTMR_TimerCompareFlag%3C%2FEM%3E%3C%2FSPAN%3E%20%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%EF%BC%89%EF%BC%9B%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20%7D%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%200.0001pt%3B%22%3E%3CSPAN%20style%3D%22font-size%3A%2010.0pt%3B%20font-family%3A%20Consolas%3B%20color%3A%20black%3B%22%3E%7D%3C%2FSPAN%3E%3C%2FP%3E%3C%2FLINGO-BODY%3E
无评分
版本历史
最后更新:
‎07-25-2016 11:09 AM
更新人: