swt1 configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

swt1 configuration

2,157 Views
mehmetkaradag
Contributor III

Dear All,

I use MPC5777C.

I am working to configure swt_1  with the configuration that I've done for swt_0. But swt_1 not working while swt_0 is working. Also i want that just swt_1 working. I mean what do I need to do to configure the swt_1 ?

I hope someone can help me, thank you.

0 Kudos
Reply
4 Replies

2,115 Views
mehmetkaradag
Contributor III

Hi again,

I have configured SWT_B same way as SWT_A but it is not starting to count. So I have seen it is configured and its register values are correct but not starting.

 thank you.

0 Kudos
Reply

2,090 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

As I have explained in :

https://community.nxp.com/t5/MPC5xxx/SWT-B/td-p/1635343

It could be debugger causing you are not seeing SWT to run, explained it in above thread.

Best regards,

Peter

0 Kudos
Reply

2,136 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

There is nothing special. Simply configure it same way as SWT_A.

Attached is my sample code.

Best regards,

Peter

 

2,113 Views
mehmetkaradag
Contributor III

Hi again, I have configured SWT_B same way as SWT_A but it is not starting to count. So I have seen it is configured and its register values are correct but not starting. thank you.

0 Kudos
Reply