sending array using i2c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sending array using i2c

1,820 Views
turkmani_11
Contributor III

hi i wrote the following code from the given example code which sends a message using i2c.

i got the massage using logic analyzer.

i want to send an array rather than 1 message, the code is :

/*****************************************************************************/
/* FILE NAME: i2c_Z4_1.c COPYRIGHT (c) NXP Semiconductors 2016 */
/* All Rights Reserved */
/* PLATFORM: DEVKIT-MPC5748G */
/* DESCRIPTION: Initializes the I2C_1 in master mode and I2C_2 in slave mode*/
/* Master sends the address and data and Slave receives both */
/* The address and the data */
/* Provide a pull-up of 3.3V via pull-up register(10k) to both */
/* SCL and SDA lines */
/* I2C_1 I2C_2 */
/* SCL: PE0: J4_16 SCL: PE9: J2_8 */
/* SDA: PE1: J4_14 SDA: PE8: J2_6 */
/*****************************************************************************/
/* REV AUTHOR DATE DESCRIPTION OF CHANGE */
/* --- ----------- ---------- --------------------- */
/* 1.0 K Shah 31 Mar 2016 Initial working version */
/* */
/*****************************************************************************/

#include "derivative.h" /* include peripheral declarations */
#include "project.h"
#include "mode.h"
#include "i2c.h"


#define KEY_VALUE1 0x5AF0ul
#define KEY_VALUE2 0xA50Ful

extern void xcptn_xmpl(void);
void peri_clock_gating(void); /* Configure gating/enabling peripheral(I2C) clocks */

void hw_init(void)
{
#if defined(DEBUG_SECONDARY_CORES)
uint32_t mctl = MC_ME.MCTL.R;
#if defined(TURN_ON_CPU1)
/* enable core 1 in all modes */
MC_ME.CCTL[2].R = 0x00FE;
/* Set Start address for core 1: Will reset and start */
MC_ME.CADDR[2].R = 0x11d0000 | 0x1;
#endif
#if defined(TURN_ON_CPU2)
/* enable core 2 in all modes */
MC_ME.CCTL[3].R = 0x00FE;
/* Set Start address for core 2: Will reset and start */
MC_ME.CADDR[3].R = 0x13a0000 | 0x1;
#endif
MC_ME.MCTL.R = (mctl & 0xffff0000ul) | KEY_VALUE1;
MC_ME.MCTL.R = mctl; /* key value 2 always from MCTL */
#endif /* defined(DEBUG_SECONDARY_CORES) */
}

/************************************ Main ***********************************/

__attribute__ ((section(".text")))
int main(void)
{
uint8_t data;
int array []={1,3,2,1,3,4,2,1,4};
int i;

xcptn_xmpl (); /* Configure and Enable Interrupts */

peri_clock_gating(); /* Configure gating/enabling peripheral(I2C) clocks */
system160mhz();
/* Sets clock dividers= max freq,
calls PLL_160MHz function which:
MC_ME.ME: enables all modes for Mode Entry module
Connects XOSC to PLL
PLLDIG: LOLIE=1, PLLCAL3=0x09C3_C000, no sigma delta, 160MHz
MC_ME.DRUN_MC: configures sysclk = PLL
Mode transition: re-enters DRUN which activates PLL=sysclk & peri clks
*/
initI2C_1(); /* I2C1 module configured as a Master and in Transmit mode */
initI2C_2(); /* I2C2 module configured as a Slave and in Receive mode */

/* Transmit Address */
transmit_addr_master_I2C_1(0xFE);
receive_addr_slave_I2C_2();

while(1)
{

transmit_data_master_I2C_1(0x01);
data = receive_data_slave_I2C_2();

if(data == 0x01)
{
SIUL2.MSCR[PA10].B.OBE ^= 1; /* Pad PA10 (10): OBE=OBE xor 1. On EVB active low DS4 LED */
data = 0;
}

}
return 0;
}

/******************** End of Main ***************************************/

void peri_clock_gating() { /* Configure gating/enabling peripheral(I2C) clocks */
MC_ME.RUN_PC[0].R = 0x00000000; /* Gate off clock for all RUN modes */
MC_ME.RUN_PC[1].R = 0x000000FE; /* Configures peripheral clock for all RUN modes */
MC_ME.PCTL[31].B.RUN_CFG = 0x1; /* I2C_1: select peripheral configuration RUN_PC[1] */
MC_ME.PCTL[32].B.RUN_CFG = 0x1; /* I2C_2: select peripheral configuration RUN_PC[1] */
}

logic analyzer:

logic analyzer.png

 

Tags (4)
0 Kudos
Reply
1 Reply

1,812 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if you want to write own code or modify this demo example you can follow section 44.7 Initialization/application information of the RM.
Also you can refer to simple i2c driver at https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5xxx-I2C-communication-driver/ta-p/1121925.

BR, Petr

0 Kudos
Reply