questions for the using of SPI about the DSPI moudle of MPC5634

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

questions for the using of SPI about the DSPI moudle of MPC5634

1,969件の閲覧回数
annycai
Contributor I

Currently,I’m engaged in a project about engine control. Now I meet some troubles in using SPI(one mode of DSPI module of MPC5634)transit commands todrive the MC33810 to finish the spark and fuel function.

 

I hope get the following answer as more as possible:

 

1. Send me some C functions about the using of SPI to finish the control between the MPC5634 and the MC33810

 

2. Or SPI examples in communication between MPC5634 and the peripherals(such as MC33810,MC33800,MC9332).

 

I am sinceresly appreciate for your information.

ラベル(1)
タグ(3)
0 件の賞賛
返信
0 返答(返信)