my bootloader jump to app err

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

my bootloader jump to app err

1,202 Views
huangchuo
Contributor I
/* Configure FCCU */
FCCU_SetProtocol(FCCU_BI_STABLE); //set Bi-Stable protocol if not in the SAFE mode

/* Init MODE ENTRY module */
MC_MODE_INIT(); /* (pll_init) Setup the MCU clocks and modes */

xcptn_xmpl (); /* Configure and Eable Interrupts */

dcache_disable();

PIT_Init();

PIT_Setup(0,50000000, 0.005);

MC33908_Init();

DSPI_Init(EEROM_DSPI_NB,MASTER,DSPI_CLK,EEROM_DSPI_BR,0);

if(Get_AppValid())
{
__asm__("e_lis %r12,0x00FB");
__asm__("e_or2i %r12,0x0004");
__asm__("e_lwz %r0,0(%r12)");
__asm__("se_mtlr %r0");
__asm__("se_blrl");
}
......

The above code runs in the bootloader main () function.

Get_AppValid () detects valid flags for applications in flash. The flags is stored at flash 0x11C0000. When the application download finished , the flags is set to 0x5555AAAA. The Get_AppValid () function check passes through assembly instructions jump to the application.

The application start address is 0x1040000,

app flash.ld 
MEMORY
{

    flash_rchw : org = 0x00FB0000, len = 0x4
   cpu0_reset_vec : org = 0x00FB0004, len = 0x4

   m_text : org = 0x1000000, len = 2048K
   m_data : org = 0x40000000, len = 256K

   int_dram : org = 0x50800000, len = 64K
}

Now after the download finished, bootloader reset, restart, run to the Get_AppValid (), jump into the APP operation. As a result, IVOR1 interrupts are generated. Single step debugging to see, the program jumped to the 0x1040000, and running 4 instructions, and then into the ivor1 interrupt.

Hope technical support can help solve. Determines whether or not to change the jump mode, or the chip needs to do relevant settings to modify the machine check function.

0 Kudos
Reply
1 Reply

969 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi

Ok, First of all it is good to know which MCU you are using.

There are plenty of them and all contains FCCU, but each FCCU implementation is different.

Peter