mpc5777c CSE load key

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mpc5777c CSE load key

ソリューションへジャンプ
2,568件の閲覧回数
InhyeokHwang
Contributor III

Hi NXP teams

I'm currently studying on cse_keyconfig_mpc5777c example code from s32 ds pa 2.1 and I found something strange in the code which I don't get it.

According to the reference manual, all M1, M2, M3, M4, M5 should be computed and used for the load key command.

But in the example code, I only can see computeM1M2M3 function inside load key command and have no idea why computeM4M5 is not being used.

When I try to find the usage of computeM4M5 in the project using ctrl+h, this function is used nowhere. 

Thanks in advance

タグ(1)
0 件の賞賛
返信
1 解決策
2,552件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @InhyeokHwang 

the thing is that M1-M3 are input parameters needed to load a key, M4-M5 values are output values.

M4-M5 values should be used to verify if a key was loaded correctly. If returned M4-M5 values match with M4-M5 values calculated offline, it's a proof that the key was loaded correctly. In the real application, it's highly recommended to do this checking, of course. Project cse_keyconfig_mpc5777c is example only, it's not implemented for some reasons.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,553件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @InhyeokHwang 

the thing is that M1-M3 are input parameters needed to load a key, M4-M5 values are output values.

M4-M5 values should be used to verify if a key was loaded correctly. If returned M4-M5 values match with M4-M5 values calculated offline, it's a proof that the key was loaded correctly. In the real application, it's highly recommended to do this checking, of course. Project cse_keyconfig_mpc5777c is example only, it's not implemented for some reasons.

Regards,

Lukas

0 件の賞賛
返信
2,549件の閲覧回数
InhyeokHwang
Contributor III

thanks for the reply. I appreciate it

0 件の賞賛
返信