mpc5674f flash erase

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mpc5674f flash erase

1,984 次查看
roganchoi
Contributor II

hello , thesesdays im trying to make some flash residence bootloader for mpc5674f

i found some reference pdf and project which is for mpc5634m and ssd driver

and below code is reference things... but it's not working

however, 5634m code is working.. i dont why and how it is working...

is there a someon who can explane to me?

/* Erase all blocks (except area occupied by bootloader) in low and mid addr space of flash array 0 */
  // it is a 5634m code 

  // lowEnabledBlocks = 0x000003F8;
  // midEnabledBlocks = 0x00000003;
 // highEnabledBlocks = 0x00000000;
  

 /* Select all blocks in low addr space except block 0  */
   #if (!RUN_IN_FLASH)
    lowEnabledBlocks = (0xFFFFFFFF >> (32 - ssdConfig.lowBlockNum));
   midEnabledBlocks = 0x00000000;
   highEnabledBlocks = 0x00000000;
   
  returnCode = pFlashErase( &ssdConfig,
                              shadowFlag,
                              lowEnabledBlocks,
                              midEnabledBlocks,
                              highEnabledBlocks,
                              (tpfNullCallback)NULL_CALLBACK );
  if ( C90FL_OK != returnCode )
  {
      return(FlashEraseError);
  }
#endif
 
 
    lowEnabledBlocks = 0x00000000;
    midEnabledBlocks = (0xFFFFFFFF >> (32 - ssdConfig.midBlockNum));
    highEnabledBlocks = 0x00000000;
    returnCode = pFlashErase( &ssdConfig, shadowFlag, lowEnabledBlocks, midEnabledBlocks, highEnabledBlocks, (tpfNullCallback)NULL_CALLBACK );
    if ( C90FL_OK != returnCode )
    {
        return(FlashEraseError);
    }

    /* Select all blocks in high addr space */
    lowEnabledBlocks = 0x00000000;
    midEnabledBlocks = 0x00000000;
    highEnabledBlocks = (0xFFFFFFFF >> (32 - ssdConfig.highBlockNum));
    returnCode = pFlashErase( &ssdConfig, shadowFlag, lowEnabledBlocks, midEnabledBlocks, highEnabledBlocks, (tpfNullCallback)NULL_CALLBACK );
    if ( C90FL_OK != returnCode )
    {
        return(FlashEraseError);
    }

标签 (1)
2 回复数

1,755 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, could you explain "it's not working"? What issue you are facing?

For MPC5674F, following SSD is supposed to be used:

https://www.nxp.com/lgfiles/Qorivva/MPC5674F_C90FL_SSD_DRV.exe 

1,755 次查看
roganchoi
Contributor II

i just want to erase flash memory expect bootloader area.....

im using SSD but , I don't understand about parameter ( ex.midEnabledBlocks = (0xFFFFFFFF >> (32 - ssdConfig.midBlockNum)))

0 项奖励
回复