mpc5121

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mpc5121

2,707件の閲覧回数
mariosan
Contributor II

Hi, I'm using the JTAG USB-TAP for MPC5121: now this tool is not more available.

Which is the tool that replaces the USB-TAB?

Is the USBTAP JTAG (PQ II/III) CWH-UTP-PPCC-HE usable?

I've not seen any MPC51xx/52xx CPU supported by that tool...

 

Thanks

Mario

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,490件の閲覧回数
a_fontquerni
Contributor I

We have a product based on MPC5121 processor.

We have ADS5121 board (Evaluation board of MPC5121 processor)  and "CodeWarrior® Development Studio for mobileGT® (Classic IDE) v9.2 for Windows and for Linux"

Recently, we purchased  CWH-CTP-BASE-HE + CWH-CTP-COP-YE

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t...

We plugged "CodeWarrior TAP" to USB and we connected with "serial ttyACM0" and "telnet 'usb0 IP'" and we read 'netstat' cmd:

core> netstat -an
Active Internet connections (servers and established)
Proto Recv-Q Send-Q Local Address           Foreign Address         State      
tcp        0      0 0.0.0.0:1100            0.0.0.0:*               LISTEN      
tcp        0      0 0.0.0.0:22              0.0.0.0:*               LISTEN      
tcp        0      0 0.0.0.0:23              0.0.0.0:*               LISTEN      
tcp        0      0 0.0.0.0:1082            0.0.0.0:*               LISTEN      
tcp        0      0 0.0.0.0:1087            0.0.0.0:*               LISTEN      
tcp        0      0 169.254.93.185:23       169.254.123.117:41218   ESTABLISHED
udp        0      0 0.0.0.0:67              0.0.0.0:*   

But we can not configure "CodeWarrior® Development Studio for mobileGT® (Classic IDE) v9.2 for Linux" to connect to "CodeWarrior TAP" ( CWH-CTP-BASE-HE + CWH-CTP-COP-YE )

We tried all port and CodeWarrior rises 'css_error=3' on 1087 and 'css_error=10' on 41474 and 41475

1) Is it possible use newer CWH-CTP-BASE-HE on "CodeWarrior® Development Studio for mobileGT® (Classic IDE) v9.2" for "MPC5121 processor" ?


2) How do we need configure "CodeWarrior® Development Studio for mobileGT® (Classic IDE) v9.2 for Linux" ?

Best regards,
Agusti

0 件の賞賛
返信

2,490件の閲覧回数
a_fontquerni
Contributor I

I attached 'telnet session welcome (version info)'

root@host:~# telnet 169.254.93.185
Trying 169.254.93.185...
Connected to 169.254.93.185.
Escape character is '^]'.

                  ####
               ##########
            ##########  ....          Freescale Semiconductor Inc.
               ####  ..........       Copyright (c) 2015
                  ..........  ####    All Rights Reserved
                     ....  ##########
                        ##########    Codewarrior TAP Firmware
                    ....   ####       Boot Loader Version 1.0.1
                 ..........             built Mon Aug 26 18:55:20 UTC 2013
              ..........  ####        OS Version 1.0.4
          ####   ....  ##########       built Thu Apr 23 22:28:59 UTC 2015
       ##########   ##########
    ##########  ....   ####           Main Board: CodeWarrior TAP (3.3V)
       ####  ..........               Probe Tip:  Power Architecture JTAG/COP
          ..........
      ####   ....
   ##########                         Note: This product uses open-source
##########                            components.  See "help license"
   ####                               for details.

core>

0 件の賞賛
返信