microsecond channel driver development

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

microsecond channel driver development

2,377 Views
wrathofhelix
Contributor I

Hello ,

I am working on developmet of MSC bus driver, but there is no reference/application note for feature CSI/TSB as downstream channel. Is there any application note/reference to implement feature CSI/TSB mode for MSC?

Thanks/Regards

0 Kudos
Reply
3 Replies

2,356 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,352 Views
wrathofhelix
Contributor I

Hello @davidtosenovjan ,

I read all related topics on community page, but I meant that I need Microsecond Channel configuration to configure DSPI. For example , common settings, frame size, chip select etc. Comments are not enough which you mentioned.  Don't you have any application note to implement this configuraton as an example? 

Thnaks/Regards

 
 
 
0 Kudos
Reply

2,311 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I think we don't have such example. „Microsecond channel“ is third-party protocol and I communication parameters should be defined by slave device. However it should be achievable by TSB extension to the DSPI module.

0 Kudos
Reply