max frequency on MPC5777C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

max frequency on MPC5777C

1,728 Views
marcellobellini
Contributor I

I would need to increase the frequency of the mpc5777c from 300mhz to 324mhz. My application works in a temperature range of 0-70 degrees.
it's possible?

0 Kudos
Reply
2 Replies

1,694 Views
marcellobellini
Contributor I

OK i try, because i have no other solution to speed up a function

0 Kudos
Reply

1,713 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

The max tested and specified frequency for this device is 300MHz. If you run it at higher we will not guarantee its correct operation as specified in datasheet.

Best regards,

Peter

0 Kudos
Reply